Escolha sua região e idioma

Ir

Menu

Distribution transformer repairs

Distribution transformers ranging from 315 kVA to 5 MVA are readily distributed across the distribution networks, forming an integral part of the overall distribution network. Upon receipt of the transformer in the factory for repair, a visual and electrical control will be performed.

Based on the scope of work and repairs generally the repair time for the distribution is short and in some cases it could be between 3-5 weeks. In some cases it may require to replace items which are not normally stock item, in those cases the lead times are adjusted after reviewing with the customer.

Scope of work

The transformer is inspected on arrival to determine the course of action and what rehabilitative actions should be performed. This can include an electrical condition assessment and visual inspection of transformer tank, expansion tank, radiators and fans and internal cleaning and inspection of the same.

Depending on size and the inspection, intervention of active part, including the repair of minor insulation damage, can be performed. Service on accessible parts such as the tap changer, bushings, oil handling, drying the active part and necessary tests are performed before returning the unit back to the customer.

Contact us

Submit your enquiry and we will contact you