Choisissez votre région et votre langue

Menu

General information:

Hitachi Energy is seeking a Site Quality Manager. The role will be based in the field at the project location. Current project location is Adelanto, California . Role requires relocation to new project site upon completion. This role is responsible for planning, organizing, leading, and monitoring all Quality work during site execution to ensure we satisfy customer expectations. This includes works undertaken internally in addition to the work performed by our subcontractors and/or partners as required for the project. The Role reports functionally to the Quality & CI Manager for Site Quality. During site execution reports operationally to the Site Manager and dotted to the PQM.

Your Responsibilities:
  • Review contractual and local requirements applicable to site quality. Review lessons learnt from previous projects and relevant project plans (e.g., SQP, SMP).
  • Review Contractor Quality Plans to ensure alignment with the Project Quality Plans and the customer requirements. Based on reviews and discussion with stakeholders identify and follow up risks and mitigations to ensure we fulfill site quality expectations.
  • Set up and educate site personnel in the quality management system including the completion system at site and ensure it is compliant with any regulatory and PG requirements as well as any applicable codes & standards.
  • Provide Quality Induction training to the site personnel. Execute and follows up the Quality Plans, master test plan and completion system status for site activities as required.
  • Review quality documentations for correctness and completeness prior approval (e.g., test certificates, checklist, etc.). Ensure that the quality control plans (ITP, ITR etc.) and any erection documentation (isometrics, procedures, etc.) provided by HVDC are effectively communicated to the site management team and the contractors.
  • Ensure that Quality Control processes are fully implemented and continuously monitored. Ensure that inspection / testing during Civil, Mechanical & Electrical erection and Commissioning are conducted, documented, checked, and validated as per the quality control system.
  • Organize and supervise acceptance testing and/or approval by customers, third parties and governmental authorities whenever required at site. Ensure that the completion system, deviation, NCR (Non-Conformance Report) System, CCRP system and any other Quality tools are fully deployed at site and that the users are adequately trained.
  • Ensure that all testing and measurement equipment used at site are listed and calibrated and that the associated calibration certificates are available. Follow up completion system at site having an overview of status regarding inspections, certifications and all outstanding works including punch list.
  • Provide Quality related site KPIs to the stakeholders whenever required. Coordinate, follow-up, and lead site inspections and support the management of punch-out items. Provide Quality inputs to the site management to support on-time and in-budget execution of the project.
  • Perform site quality inspection of goods coming to site and report any deviations according to the project regulations. Follows up that handling, storage of delivered material and equipment are in accordance with the manufacture's guidelines and the SQP.
  • Ensure that the ITP/ITR are applied by the sub-contractor and its subcontractors including the compliance with the Hold points and Witness points. Ensure site quality documentation is generated, distributed, updated, and archived in accordance with the Management system and completion system requirements. Deploy Site Quality audit program (including contractor audits and internal audits).
  • Participate in internal and contractor quality audits as per the Site Quality audit program. Assist and coordinate any planned external site related audits. Monitor contractor compliance with Quality requirements and implement corrective actions whenever required.
  • Follow up the adherence and governance of the quality management system at site. Support in identifying lessons learnt and contribute with input to the Lesson Learn Process.
  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background:
  • Bachelor's degree in technical, engineering, quality management and a 5+ years of construction quality site experience OR High School Diploma / GED and a 9+ years of construction quality site experience.
  • Candidate must already have a work authorization that would permit them to work for Hitachi Energy in the United States.
  • Willingness to relocate for the duration of the project wherever the construction site is located. (Current project plan; two years in Lewiston Maine then other state in continental United States.)
  • Power or energy industry experience highly advantageous. Track record and proven capability in Change Management, managing internal project/program in large and complex organization.
  • Experience in process management ideally in project business, preferably in the energy or automation industry, or other quality and process-oriented industries. Continuous Improvement experience. L6S Belt. Capacity to communicate, result oriented, speed in execution, openness and listen to others.
  • Test coordination experience is required.
  • ISO9001 knowledge is required.
  • Certified auditor is plus.
  • Knowledge and experience on construction codes / standards.
  • Computer skills and knowledge of completion systems.
  • English fluency (written + spoken).

Lieu Los Angeles, California, United States of America
Type d'emploi Full time
De l'expérience Experienced
Fonction du poste Quality Management
Contrat Regular
Date de publication 2024-11-05
Numéro de réference R0064224

À propos de Hitachi Énergie

Hitachi Énergie est un chef de file technologique mondial voué à la promotion d’un avenir énergétique durable pour tous. Nous servons des clients dans les secteurs des services publics, de l'industrie et des infrastructures avec des solutions et des services innovants tout au long de la chaîne de valeur. Avec nos clients et nos partenaires, nous sommes pionniers en matière de technologies et permettons la transformation numérique nécessaire pour accélérer la transition énergétique vers un avenir carboneutre. Nous faisons progresser le système énergétique mondial pour qu'il devienne plus durable, plus flexible et plus sûr, tout en équilibrant les valeurs sociales, environnementales et économiques. Hitachi Énergie est forte d’une expérience avérée et dispose d’une base installée inégalée dans plus de 140 pays, Avec son siège social établi en Suisse, la société emploie plus de 45 000 personnes dans 90 pays et génère des volumes d’affaires de plus de 13 milliards de dollars US.
www.hitachienergy.com

Hitachi Energie est un employeur qui prône l'égalité des chances en matière d'emploi et l'action positive, et qui encourage la diversité sur le lieu de travail. Nous vous invitons à poser votre candidature et tenons à ce que vous sachiez que tous les candidats qualifiés seront pris en considération pour un emploi sans distinction de race, de croyance, de couleur, d'ascendance, de religion, de sexe, d'origine nationale, de statut de citoyen, d'âge, d'orientation sexuelle, d'identité de genre, de handicap, d'état civil, de statut de congé médical familial, de statut d'ancien combattant protégé ou de toute autre caractéristique protégée par la loi. Pour plus d'informations sur vos droits en matière d'égalité des chances en tant que candidat, veuillez consulter le site web suivant : ici. Les personnes qualifiées souffrant d'un handicap peuvent demander un aménagement raisonnable si leur handicap les empêche d'utiliser le site de carrière de Hitachi Énergie ou les limite dans leur capacité à y accéder. Vous pouvez demander des aménagements raisonnables en appelant un représentant des ressources humaines de Hitachi Énergie au 1-888-504-2007 ou en envoyant un courriel à : [email protected]. Notez que les CV et les candidatures envoyés à ces coordonnées ne seront pas acceptés.