Choose your region and language

Go

Menu

Ireland. Woodland. Interiors, exteriors and details from the site in Woodland, Ireland.

East West Interconnector

Customer Goal

The EirGrid East-West Interconnector Project (EWIP) has been built in order to facilitate the cross-border transportation of power between Britain and Ireland.

The integration of an HVDC system with the AC network required system studies to evaluate its contribution to network operation enhancement. The expert team from Power Consulting has been in charge of these studies.

Addressing the issue

System stability and damping studies have been performed using PSSE for the Irish grid. The results showed stable operation without the need of a damping controller. Additionally, the HVDC operation during emergency conditions such as disconnection of important lines and/or generators has been evaluated for the Irish grid.

Some studies were performed in PSCAD/EMTDC, using very detailed models for the HVDC system. For these studies, reduced network models were required. The AC network reductions for the Irish grid have been performed in PSSE and further implemented in PSCAD/EMTDC.  

Sub-synchronous interaction between the HVDC and the nearby generators is a well known effect and therefore the interaction levels have been calculated for both the Irish and British grid by means of PSSE. Further, studies were performed in PSCAD /EMTDC with very detailed HVDC and generator models for some of the generators units on the Irish side. The HVDC has been tuned at these studies in order to avoid interaction problems.

Customer’s benefits

By connecting to the British grid, Ireland will gain access to the European transmission network and respective markets.

The interconnector will enable Ireland to import and export power to and from Britain, thereby creating a more competitive market and reducing customer prices. It will also help Ireland to meet its target of one-third electric power by renewable resources by 2020.

Main data

Commissioning year: 2013
Power rating: 500 MW
No of circuits: 1
AC Voltage: 400 kV
DC Voltage: ±200 kV
Length of DC underground cable: 2 x 75 km
Length of DC submarine cable: 2 x 186 km
Main reason for choosing HVDC Light®: Length of land and sea cables, controllability, black start and active reactive power support
Application: Interconnecting grids