Choose your region and language

Go

Menu

On-site low frequency heating (LFH) drying

Virtually all moisture in a transformer can be found in the fixed insulation material. The significance of water content is paramount: laboratory samples suggest that a humidity of 3-4 percent may increase the degradation rate of paper by a factor of 10 or more, compared to dry paper.

This underlines the importance of assessing both moisture and temperature of the insulation system. Temperature and vacuum are the main factors for drying speed and drying quality.

For optimized drying the transformer should be heated at the same time as vacuum is applied (as is done during the vapor phase process). With the combination of the low frequency heating (LFH) technique and hot oil spray or hot oil circulation, this can also be achieved on-site.

The low frequency voltage is necessary in order to reduce the applied voltage on the transformer when it is under vacuum. The reason is that the breakdown voltage of the insulation system is much lower under vacuum than under atmospheric pressure. This is also known as the Paschen's law.

In order to prevent hotspots during drying (due to reduced cooling), the applied current for heating power transformers should not exceed 50% of the nominal current. Consequently, the copper losses will be no more than Ľ of the nominal losses and the risk of potential hot spots at points with higher resistance will be negligible.

Scope of work

Plant and process concept

In order to heat up both the low and high voltage windings, a frequency of approx. 1 Hz is applied to the transformer.

With the combination of LFH drying and conventional hot oil spray method, the whole transformer can be heated uniformly. The LFH system heats the windings from the inside and the hot oil spray supports the heating process by heating outer parts of the insulation system.

Onsite LFH Drying - diagram

Contact us

Submit your enquiry and we will contact you