Scegli la tua regione e lingua

Vai

Menu

Mission Statement

Project Engineering focuses on designing, communicating, and implementing an operational plan for completing an engineering-based project including: Preparing designs, project controls and specifications, schedules, cost estimates, production, transportation, installation, testing and/or commissioning of new infrastructure, facilities, equipment, etc. Monitoring progress and performance against the project plan; taking action to resolve operational problems and minimize delays. Identifying, developing, and gathering the resources necessary to complete the project. May include preparing engineering standards, designs and work specifications; developing project schedules, budgets and forecasts; and selecting materials, equipment, project staff, and external contractors A Senior Professional (P3) applies advanced knowledge of job area typically obtained through advanced education and work experience. Responsibilities may include: Managing projects / processes, working independently with limited supervision. Coaching and reviewing the work of lower level professionals. Problems faced are difficult and sometimes complex.

Your responsibilities

  • Create a Base Design with all necessary Concepts. 
  • Verify the implemented Base Design in the Detail Design (Bay and Station level Engineering). 
  • Technical Coordination and Lead for the project team during the project execution phase (Detail Design, Manufacturing, Testing, Commissioning). 
  • Technical coordination for FAT. 
  • Responsible for ensuring that specification is fulfilled in respect of the technical offer. 
  • Contribute to the improvement of the Net-margin including upsales, etc. 
  • Ensure project execution is carried out fulfilling internal processes and guidelines. 
  • Ensure experience and learnings during the project execution are shared with colleagues within the same unit (Sales, B&P, PMs, Engineering, Testing, Commissioning). 
  • Project execution for complex projects (E.g. Retrofit, Fast Track Projects, Turn Key Projects, etc.) 
  • Contribute to identifying market-compliant, low-risk technical solutions and efficient project setup (E.g. Organization, Communication, Sub-supplier). 
  • Should have knowledge of Generator, Line, Transformer, Busbar protection relays, and Bay control units 
  • Should have worked on IED configuration tools like PCM600, DIGSI, Agile studio, Easergy Studio, etc., 
  • Should have worked on MicroSCADA for SAS & DMS, Gateway and Remote HMI applications, etc., 
  • Work experience on 800xA for HMI, Load shedding, Generator shedding application, etc., will be an added advantage 
  • Should have working knowledge of Protocols such as IEC61850, Modbus, IEC-104, IEC-101, DLMS etc., 
  • Should have a working knowledge of Cyber Security for designing Substation Automation/Network control centers. 
  • Living Hitachi Energy core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background:

  • BE/B.Tech - Electrical or Electronics Engg. with 5 – 8years of relevant experience.
  • Proficiency in both spoken & written English language is required.

Sede Bengaluru, Karnataka, India
Tipo di lavoro Full time
Esperienza Experienced
Funzione lavorativa Engineering & Science
Contratto Regular
Data di pubblicazione 2024-10-24
Numero di riferimento R0063284

Hitachi Energy

Hitachi Energy è un leader tecnologico globale che promuove un futuro energetico sostenibile per tutti. Collaborando con clienti e partner, rende il sistema energetico mondiale più sostenibile, flessibile e sicuro. 

Più di 45.000 persone in 90 paesi ogni giorno lavorano con uno scopo e utilizzano i loro diversi background per sfidare lo status quo. Candidati e diventa  parte di un team globale che apprezza una semplice verità: Diversity + Collaborazione = Grande Innovazione.