地域と言語を選択してください

メニュー

Configuration and testing Engineer

Mission Statement

Plan, prepare and coordinate pre-commissioning/commissioning/start-up activities leading to project completion. Develop and ensure adherence to a detailed commissioning schedule and plan, covering all aspects of pre-commissioning and start-up phases through to handover. Prepare and/or update a comprehensive commissioning manual. Develop a reporting structure and accountabilities for the commissioning team. Plan and coordinate the commissioning/start up schedule and necessary work with third party providers. Develop pre-commissioning test procedures and documentation. Correct any deficiencies found. Ensure compliance and progress reports are produced in accordance with client and legislative requirements. Liaise with government agencies where required to obtain necessary approvals prior to start-up. Prepare client acceptance forms and ensure satisfactory sign-off is obtained. Develop comprehensive quality, environment and safety commissioning plans. An Experienced Professional (P2) applies practical knowledge of job area typically obtained through advanced education and work experience. May require the following proficiency: Works independently with general supervision. Problems faced are difficult but typically not complex. May influence others within the job area through explanation of facts, policies and practices.

Your responsibilities

  • As a testing and configuration engineer, carrying out the configuration of IED’s in line with project requirements and testing of Control and relay panels, Substation automation system delivered and actively contribute in the testing team of Grid Automation Systems.
  • Execute the project IED’s configurations and testing safely following all safety standards of HEIL as well as customer. Reports Hazards, Near Misses at working location back to office for records and further improvement.
  • Ensure that customer relations are managed in an optimal way.
  • Carryout the Configurations of IED’s and testing the Control, Protection and SAS panels as per the documented process description and checklists. Continuous interactions with testing Lead and expert help to carry out the testing works effectively.
  • Report the Configuration and testing project status testing progress & testing plan to testing Lead. Ensure efficient use of the testing assets like Test kits, Tools etc.
  • Ensures project information of any project is fully taken from testing lead and get all IED’s fully configured and tested in line with customer approved drawings and ready for the project specific testing activities before offering the projects to customer during FAT.
  • Handing over the marked-up drawings to engineering for preparing the As-build drawing and onward submission to customer to close the project.
  • Handover the final testing backup CD's, Micro SCADA system backup, IET workplace backup and other backup as per the checklist to lead.
  • Actively and regularly (Compulsory for every project) provides feedback to Engineering Project Management, manufacturing and quality in way that ensures re-usage of experience.
  • Follow the key process like Test procedures, Time sheets and STAART Meetings.
  • Ensure the installed base numerical relays are maintained with minimum revisions by continuously updating the older revisions.
  • Ensure the usage of the latest tools and latest software versions during project IED configurations and testing.
  • Continuous learning & acquiring expertise in various protection schemes and Automation system to achieve the higher growth in ‘learning curve’.
  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background:

  • Candidate should have BE/B.Tech - Electrical or Electronics Engineering with 8 – 12 years of relevant experience.
  • Should have a minimum of 3 years of experience in testing and commissioning of control and relay panels in projects above 132kV Voltage levels.
  • Should have good knowledge on Power system.
  • Should have hands on experience with 3 Phase injection test kits like Omicron, Doble, Megger, Ponova etc…
  • Should have good knowledge on understanding the schematics of control and relay Panels, primary equipment interlocks.
  • Should be ready for frequent travels all over India and overseas wherever assigned.
  • Should have e good knowledge on configuration of HEIL IED’s and competitors IED’s in line with project requirements.
  • Should have a minimum of 3 years of experience in commissioning of SAS with IEC61850 standards, IEC101, IEC104, OPC and Modbus protocols.
  • Should have good knowledge on IEC61850 standards, Ethernet, Serial communications.
  • Should have good knowledge on communication protocols such as Modbus, DNP 3.0, IEC 101, IEC 104, OPC,
  • Should have competency on networking, configuration of managed Ethernet switches.
  • Should have hands on experience on Protocol analyzers like IEC browser and network analyzer tools like wire sharks.
  • Proficiency in both spoken & written English language is required.

就業場所 Bengaluru, Karnataka, India
職種 Full time
体得 Experienced
職務 Engineering & Science
契約 Regular
発行日 2024-05-29
整理番号 R0033212

日立エナジーについて

日立エナジーは、持続可能なエネルギーの未来へ向けた取り組みを加速する、グローバルな技術リーダーです。さまざまな分野のお客さまに、バリューチェーン全体にわたる革新的なソリューションとサービスを提供するとともに、お客さまやパートナーとの協創により、カーボンニュートラル実現に向けたエネルギー転換に必要な、デジタル技術を活用した変革を実現します。

日立エナジーは、全世界90カ国に約45,000人の従業員を擁しており、それぞれが事業の継続に向け、異なる背景を生かし目的を持ちながら働いています。“ダイバーシティ+コラボレーション=優れたイノベーション”という基本的な理念を重んじる日立エナジーのグローバルなチームが、あなたをお待ちしています。