地域と言語を選択してください

メニュー

Quality Inspector for Supply Quality & Development

Mission statement:

Your role is to make sure that production of Transformers’ metal fabrication on Chinese soil is done according to Hitachi Energy Quality requirements. This will require daily presence at suppliers, thus is a site working location job. The job might require flexibility on working schedule. Along with this role you will also focus on Welding topics, Product qualifications, Inspections, as well as non-conformity resolution. You will participate to improve the situation at current suppliers as well as develop new ones to meet Quality and OTD (On Time Deliveries) targets.   

Your responsibilities:

  • Your role will be to help the team to ensure that the special process Welding is organized and executed correctly at suppliers in compliance with the actual relevant standards as well as Hitachi Energy internal procedures: apply and enforce the standard for welding quality in railway: EN 15085 CL1 and general welding quality: ISO 3834-2 standards, as well as other internal guidelines.

  • You will support the development of welded parts according to Hitachi Energy milestones process of metal fabrication (welding, painting, design and dimensional part) and follow up until the official validation of the product by the customer and participate in PMR (Pre-Manufacturing Review) and FAI (First Article Inspection),

  • Your role will be to ensure Safety and Quality of the railway components being delivered to Hitachi Energy; this means following the product fabrication during development phase but also in serial production, inspection of the parts at suppliers will take place during prefabrication, fabrication and once manufacturing is finished in order to get final inspection validated in the first time and no non-conformity for the final product.

  • You will alert if any deviation is noticed and organize countermeasures at suppliers, when needed you will define rework procedure (in line with the rest of the Welding Coordination team) and you will monitor the good execution.

  • You will review documentation related to Quality & Welding such as: Quality & Inspection Plan, Manufacturing sequence, welder qualifications, NDT (Non-Destructive Testing), jigs and tooling, etc., you will also check the workshop & work environment: welding stations, traceability of raw material and filler material, welding generators, etc.

  • Along with welding requirements, you will make sure that dimensional and painting requirements are fulfilled and have to perform some measurements yourself to cross check the supplier process.

  • You will be participating to the resolution of NCR (Non-Conformity Report), Addressing RCA (Root Cause Analysis), making sure that the relevant corrective as well as preventive actions are taken at suppliers. You will participate to the collect and analysis of some KPI (Key Performance Indicators) for Quality & OTD (On Time Deliveries), actively participate to maintaining and developing the supplier base of Hitachi Energy in China (according to the strategy defined in Hub EUC), this will require follow-up audits at current suppliers as well as new audit at potential suppliers and during supplier development phase you will be required to work hand in the hand with the supplier to bring them up to speed regarding the expected requirements.

  • Living Hitachi Energy's core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background:

  • Require IWT or IWS (International Welding Technician or Specialist) would be preferred.

  • VT (Visual Testing) level 2 is mandatory if no IWT or IWS degree.

  • Experience in welding/painting and related inspection process would be preferred.

  • Ability to communicate with different hierarchical levels of people internally at Hitachi Energy as well as externally.

  • Good command in English B1 / Chinese B2.

就業場所 Changsha, Hunan, China
職種 Full time
体得 Experienced
職務 Engineering & Science
契約 Regular
発行日 2024-07-20
整理番号 R0056503

日立エナジーについて

日立エナジーは、持続可能なエネルギーの未来へ向けた取り組みを加速する、グローバルな技術リーダーです。さまざまな分野のお客さまに、バリューチェーン全体にわたる革新的なソリューションとサービスを提供するとともに、お客さまやパートナーとの協創により、カーボンニュートラル実現に向けたエネルギー転換に必要な、デジタル技術を活用した変革を実現します。

日立エナジーは、全世界90カ国に約45,000人の従業員を擁しており、それぞれが事業の継続に向け、異なる背景を生かし目的を持ちながら働いています。“ダイバーシティ+コラボレーション=優れたイノベーション”という基本的な理念を重んじる日立エナジーのグローバルなチームが、あなたをお待ちしています。