Selecciona tu región e idioma

Menú

Tender Phase: 

  • Delivering Tender Documentation (Bid-submission) to Customer with the inputs from Lead Engineers, Tender Leader and Dept. Head’s. 
  • Profile & upload Drawing files, Manuals, Test Reports, Calculations, etc. required for the Bid-submission from internal and Suppliers into the Database or common drive and various tools like PDL and Binder. 
  • Proper follow-up with other departments to submit the documents. 
  • Organize the files in a folder structure in the softcopy Binders. 

Project Phase: 

  • Should have experience in contract reading and understand the Customer documentation requirements 
  • Check & upload the Drawing files, Manuals, Test Reports, Calculations, etc. from Engineers and the SubSuppliers 
  • Upload the documents into the Document Management System (EDMS) 
  • Maintain the complete Project Documentation Status 
  • Communicate with Project Manager and Departments for Clarifications and Suggestions 
  • Proper follow-up with other departments to submit the documents 
  • Distribute the documents to various departments for Review & Approval 
  • Send the documents by Transmittal for Customer Review & Approval 
  • Adding the documents into e-Room (web-based database, Easy access for the members in different locations) 
  • Organize the files in a folder structure in the softcopy Binder 
  • Print out the drawings as hard copies and insert them into binders, if needed 
  • (This is the installation and Final Plant documentation) and send it to respective sites 
  • Check & upload updated drawing files (updated due to possible changes during the installation on-site) and all the above steps will be followed for new revisions, As-Built documents are printed out as hard copies and insert into binders and send to respective sites (This is the As-Built Documentation) 
  • After the Customer Approval, hand over the Project to After Sales Department 

Ubicación Chennai, Tamil Nadu, India
Tipo de empleo Full time
Experiencia Entry Level
Función laboral Project | Program Management
Contrato Regular
Fecha de publicación 2024-09-05
Número de referencia R0022525

Sobre Hitachi Energy

Hitachi Energy es un líder tecnológico mundial que está promoviendo un futuro energético sostenible para todos. Prestamos servicios a clientes de los sectores de servicios públicos, industria e infraestructuras con soluciones y servicios innovadores en toda la cadena de valor. Junto con clientes y socios, somos pioneros en tecnologías y facilitamos la transformación digital necesaria para acelerar la transición energética hacia un futuro neutro en carbono.

Empleamos a unas 45.000 personas en 90 países que cada día trabajan con un propósito y utilizan sus diferentes orígenes para desafiar el status quo. Te invitamos a presentar tu candidatura hoy mismo y a formar parte de un equipo global que aprecia una simple verdad: Diversidad + Colaboración = Gran Innovación.