Hitachi ABB Power Grids to supply transformers to Indian Railways

Press Release | Zurich, Switzerland | 10.03.2021 | 2 min read

The global technology leader will support India’s mission to make Indian Railways a net-zero carbon emitter by 2030

Hitachi ABB Power Grids in India has won orders worth about $23 million to power electric freight locomotives for Indian Railways, contributing to the ongoing modernization of the fourth-largest rail network in the world.   

Hitachi Power Grids in India, which is listed on the stock exchange as “ABB Power Products and Systems India Limited”, won the orders from the Government of India’s electric locomotive manufacturer Chittaranjan Locomotive Works (CLW) and the Central Organization for Rail Electrification (CORE).

For CLW, Hitachi ABB Power Grids will deliver traction transformers for one of Indian Railways’ most successful class of locomotives, the WAG 9, which was developed in response to strong growth in the rail freight transportation sector; for CORE, it will supply trackside transformers.

Indian Railways is aiming to create a future-ready railway system, bringing down logistics costs for industry and supporting the Make-in-India initiative. This plan aligns with the government’s goal of achieving 100 percent rail electrification by December 2023 and making Indian Railways a net-zero carbon emitter by 2030.

“These orders are a source of immense pride for us at Hitachi ABB Power Grids. They advance our vision of playing a pivotal role in rail electrification in India and enabling improvements in rail safety, capacity and speed,” said N Venu, Managing Director, Hitachi ABB Power Grids in India. “Such partnerships will help lower our dependence on imported fossil fuel and reduce both fuel costs and carbon emissions for the Indian Railways,” he added.

Hitachi ABB Power Grids will deliver trackside transformers rated 132 kV (kilovolt) to CORE and traction transformers rated 25 kV to CLW. The trackside transformers reduce power voltage from the utility power network to a suitable level before feeding it to the railway catenary conductors. Traction transformers route power from the catenary  for essential train functions such as traction, lighting, ventilation, braking, signaling and communication.

About Hitachi Energy

 

Hitachi Energy is a global technology leader that is advancing a sustainable energy future for all. We serve customers in the utility, industry and infrastructure sectors with innovative solutions and services across the value chain. Together with customers and partners, we pioneer technologies and enable the digital transformation required to accelerate the energy transition towards a carbon-neutral future. We are advancing the world’s energy system to become more sustainable, flexible and secure whilst balancing social, environmental and economic value. Hitachi Energy has a proven track record and unparalleled installed base in more than 140 countries. Headquartered in Switzerland, we employ around 38,000 people in 90 countries and generate business volumes of approximately $10 billion USD.

Contacts

Manashwi Banerjee

Region Communications Manager

Mobile phone number: +917259766881

Toutes les actualités