The AI Paradox: Why Domain Experts Become More Valuable in the Age of AI
Blog Post | 16.10.2026 | 5 min read | Bo Yang
Blog Post | 16.10.2026 | 5 min read | Bo Yang
Every major technology wave promises to make expertise less important. Calculators were supposed to reduce the need for mathematicians. Low-code platforms were supposed to reduce the need for software engineers. Now AI is supposed to reduce the need for domain experts.
The story goes something like this:
“AI can write code.”
“AI can design products.”
“AI can draft contracts.”
“AI can analyze engineering reports.”
So naturally, expertise becomes less important. I don’t think that’s what’s happening. In fact, I believe the opposite is true.
That sounds counterintuitive. But once you understand how modern AI works, it makes perfect sense.
Large language models are extraordinary at generating options. Ask AI to design a power system. It can propose five architectures.
Ask it to debug software. It may suggest ten possible causes.
Ask it to write a product requirements document. It can generate something that looks remarkably complete.
But AI doesn’t know which answer is correct. It knows which answers are plausible. That distinction matters. AI is incredibly good at expanding the solution space. Humans still have to shrink it.
This becomes obvious in engineering. Suppose an AI proposes three approaches for integrating a new substation into an existing network.
All three sound technically reasonable. Only one satisfies local operating constraints. Only one complies with utility standards. Only one can actually be built within budget.
To someone without domain expertise, all three may look equally convincing. To an experienced engineer, two can be eliminated in minutes.
The AI didn’t replace expertise. It made expertise more valuable.
One of AI’s greatest strengths is speed. Instead of exploring one design in a day, a team can evaluate twenty. Instead of writing one prototype in a month, they can build five. Instead of reviewing one option, they can generate fifty.
That sounds like a productivity miracle. But there’s a hidden consequence.
When you generate more options, you also generate more bad options. The faster AI produces ideas, the more often someone must ask: Which of these should we trust?
That someone is usually a domain expert.
Over the past year, I’ve been experimenting with AI-native product development.
The productivity gains have been real. We build prototypes faster. We iterate faster. We explore more ideas than we ever could before. But we’ve also learned something unexpected.
The biggest failures rarely came from AI producing bad code. They came from AI producing reasonable assumptions that happened to be wrong.
The developer accepted them because they sounded convincing. The product manager accepted them because they looked complete. Only when someone with deep domain expertise reviewed the design did the hidden problems become obvious. AI accelerated the work. It also accelerated the mistakes.
For years, engineering organizations were constrained by implementation.
Writing code took time. Building prototypes was expensive. Documentation was slow.
AI changes that equation.
Implementation is becoming dramatically cheaper. As implementation costs fall, something else becomes the bottleneck. Judgment. Knowing which feature matters. Knowing which assumption is valid. Knowing when AI is confidently wrong.
The scarce resource is no longer typing. It’s deciding.
One misconception I hear often is that AI turns junior engineers into senior engineers.
I don’t think that’s true.
AI can absolutely make junior engineers more productive. It can explain unfamiliar concepts, generate examples, suggest architectures, and help navigate large codebases.
That’s enormously valuable. But productivity and judgment are not the same thing.
A senior engineer doesn’t add value because they type faster. They add value because they’ve seen systems fail. They recognize hidden constraints. They know which trade-offs matter.
AI can accelerate learning. It cannot compress years of operational experience into a single prompt.
Many companies are investing heavily in AI tools. Far fewer are investing in the people who know how to evaluate AI’s output. That may become one of the biggest organizational mistakes of this decade.
As AI becomes more capable, organizations won’t need fewer domain experts. They’ll need domain experts who can review ten AI-generated solutions instead of building one from scratch. Their role shifts from creator to evaluator. Ironically, that may be even more valuable.
For years, organizations competed on execution.
Who could build faster? Who could ship more features? Who could hire more engineers?
AI is changing the competition. Execution is becoming cheaper. Judgment is becoming more valuable.
The organizations that win won’t necessarily have the best AI. They’ll have the people who know when the AI is right—and when it isn’t.
People often ask whether AI will replace domain experts.
I think that’s the wrong question.
A better question is: Who gets the most value from AI?
The answer is surprisingly simple. The people who already understand the problem. Because AI doesn’t replace expertise. It amplifies it. The better your judgment, the more value you extract from AI.
And in a world where everyone has access to increasingly powerful models, judgment-not generation-may become the rarest competitive advantage.