Wählen Sie Ihre Region und Ihre Sprache

Los

Menü

Quality Inspector for Supply Quality & Development

Mission statement:

Your role is to make sure that production of Transformers’ metal fabrication on Chinese soil is done according to Hitachi Energy Quality requirements. This will require daily presence at suppliers, thus is a site working location job. The job might require flexibility on working schedule. Along with this role you will also focus on Welding topics, Product qualifications, Inspections, as well as non-conformity resolution. You will participate to improve the situation at current suppliers as well as develop new ones to meet Quality and OTD (On Time Deliveries) targets.   

Your responsibilities:

  • Traction tanks are safety related products and require some dedicated processes and requirements, your role will be to help the team to ensure that the special process Welding is organized and executed correctly at suppliers in compliance with the actual relevant standards as well as Hitachi Energy internal procedures: apply and enforce the standard for welding quality in railway: EN 15085 CL1 and general welding quality: ISO 3834-2 standards, as well as other internal guidelines.

  • You will support the development of welded parts according to Hitachi Energy milestones process of metal fabrication (welding, painting, design and dimensional part) and follow up until the official validation of the product by the customer and participate in PMR (Pre-Manufacturing Review) and FAI (First Article Inspection),

  • Your role will be to ensure Safety and Quality of the railway components being delivered to Hitachi Energy; this means following the product fabrication during development phase but also in serial production, inspection of the parts at suppliers will take place during prefabrication, fabrication and once manufacturing is finished in order to get final inspection validated in the first time and no non-conformity for the final product.

  • You will alert if any deviation is noticed and organize countermeasures at suppliers, when needed you will define rework procedure (in line with the rest of the Welding Coordination team) and you will monitor the good execution. You will review documentation related to Quality & Welding such as: Quality & Inspection Plan, Manufacturing sequence, Welder qualifications, NDT (Non-Destructive Testing), jigs and tooling, etc., you will also check the workshop & work environment: welding stations, traceability of raw material and filler material, welding generators, etc.

  • Along with welding requirements, you will make sure that dimensional and painting requirements are fulfilled and have to perform some measurements yourself to cross check the supplier process. You will be participating to the resolution of NCR (Non-Conformity Report), Addressing RCA (Root Cause Analysis), making sure that the relevant corrective as well as preventive actions are taken at suppliers.

  • You will participate to the collect and analysis of some KPI (Key Performance Indicators) for Quality & OTD (On Time Deliveries), actively participate to maintaining and developing the supplier base of Hitachi Energy in China (according to the strategy defined in Hub EUC), this will require follow-up audits at current suppliers as well as new audits at potential suppliers and during supplier development phase you will be required to work hand in the hand with the supplier to bring them up to speed regarding the expected requirements.

  • Living Hitachi Energy's core values of safety and integrity, which means taking responsibility in own project action in the site.

Your background:

  • You hold a degree.

  • Require IWT or IWS (International Welding Technician or Specialist) would be preferred.

  • VT (Visual Testing) level 2 is mandatory if no IWT or IWS degree.

  • Experience in welding/painting and related inspection process would be preferred.

  • Ability to communicate with different hierarchical levels of people internally at Hitachi Energy as well as externally.

  • Good command in English B1 / Chinese B2.

Ort Datong, Shanxi, China
Jobtyp Full time
Erfahrung Experienced
Position Engineering & Science
Vertrag Regular
Veröffentlichungsdatum 2024-03-14
Referenznummer R0045298

Über Hitachi Energy

Hitachi Energy ist ein weltweit führendes Technologieunternehmen, das sich für eine nachhaltige Energiezukunft für alle einsetzt. Wir bedienen Kunden aus den Bereichen Versorgung, Industrie und Infrastruktur mit innovativen Lösungen und Dienstleistungen entlang der gesamten Wertschöpfungskette. Gemeinsam mit unseren Kunden und Partnern leisten wir Pionierarbeit bei der Entwicklung von Technologien und ermöglichen den digitalen Wandel, der notwendig ist, um die Energiewende hin zu einer klimaneutralen Zukunft zu beschleunigen.

Wir beschäftigen mehr als 40.000 Menschen in 90 Ländern, die sich jeden Tag dafür einsetzen, den Status quo zu hinterfragen und ihre unterschiedlichen Hintergründe zu nutzen. Bewerben Sie sich noch heute und werden Sie Teil eines globalen Teams, das überzeugt ist: Vielfalt + Zusammenarbeit = Innovation.