Chumphon
Customer Story | 1 min read
SVC for voltage control and improvement of stability
Customer Story | 1 min read
SVC for voltage control and improvement of stability
This SVC was supplied by Hitachi Energy and has been in operation since 1987. The dynamic operating range is from 60 Mvar capacitive to 20 Mvar inductive.
The SVC is an addition at the Chumphon Substation located along the 115 kV tie line approximately half way between Surat Thani and Prachuap Khiri Khan.
The main purpose of the compensator is to control the voltage in the 115 kV busbar at Chumphon.
Before the advent of the SVC, conventional switched capacitor banks and reactors were used on the 22 kV level for reactive power control but no means for dynamic voltage control existed on the 115 kV level.
| Main data | |
|---|---|
| System | SVC |
| Commissioning year | 1985 |
| Controlled voltage | 115 kV |
| SVC rating | 20 Mvar (inductive) to 60 Mvar (capacitive) |
| Control system | 3-phase voltage control by means of a voltage regulator |
| Thyristor valve | Water cooled with outdoor dry type air/water heat exchanger |