Hitachi Energy expands its Tropos industrial wireless portfolio

Press Release | Zurich, Switzerland | 27.02.2024 | 3 min read

  • Newly launched TRO670 hybrid router widens support for smart grid and Industrial Internet of Things (IIoT) applications.
  • Enables seamless network extension with backward compatibility across the entire Hitachi Energy wireless product line.

Hitachi Energy launches the TRO670 hybrid wireless router, the latest addition to its TRO600 series of high-throughput and low-latency industrial wireless communications devices to support a host of smart grid and Industrial Internet of Things (IIoT) applications.

The TRO670 incorporates multiple wireless technologies and fiber communication in a ruggedized router, enabling secure, reliable, and flexible wireless communications even in remote and harsh environments. In addition, backward compatibility across the Hitachi Energy wireless product line ensures organizations can extend their communications network without replacing existing infrastructure.

The latest router in the TRO600 series enables utilities, oil and gas companies, and mining operators to establish and expand a unified communications network for the collection and analysis of data from distributed assets.

“Connecting assets scattered across remote or hard-to-reach areas can be difficult due to connectivity limitations, often requiring additional expensive infrastructure, such as cellular towers, to ensure reliability and resiliency of the network,” said Claus Vetter, Head of Automation and Communication at Hitachi Energy. “The TRO670 can be installed in harsh environments on existing outdoor infrastructure to provide reliable yet cost-efficient ways to extend the connectivity of the operating network.”

Hybrid networks enhance reliability, flexibility, and coverage

A hybrid converged network can combine private or public cellular, third-party radios, and broadband mesh, offering versatility and allowing the grid to adapt to different communication needs and scenarios. Cellular communications enable always-on connectivity for energy management and power distribution operations, and broadband mesh ensures a robust wireless connection, enhancing communication reliability and availability. This allows flexibility in network design and optimizes coverage, enabling critical applications such as asset performance management (APM), asset monitoring, grid modernization initiatives, and automated meter reading under a single unified network management system.

The TRO670 features a multi-layer security architecture from the core to the edge. Its certificate-based Industrial Internet of Things (IIoT) security leverages public key infrastructure (PKI) to authenticate entities and create secure tunnels across public and private infrastructure. Further, security capabilities are automatically rolled out and extended as customers' networks expand.

The TRO600 series routers empower customers with enhanced performance, ensuring optimal connectivity for modern smart grid and smart city applications. From streamlined distribution to outage management systems and dispatch, the TRO670 enables efficient operations. Additionally, it supports diverse applications like intelligent transportation systems, EV charging infrastructure, kiosks, CCTV, and smart buildings, providing customers with a comprehensive and versatile communication solution.

Hitachi Energy will showcase the TRO670 series at Distributech 2024, hosted at the Orange County Convention Center in Orlando, Florida, from February 27-29, 2024.

 

Notes to editors

Key features of TRO670
 

  • Integrates multiple communication protocols, including public and private 4G cellular, broadband mesh (2.4GHz and 5GHz), and Wi-Fi access points
  • Enables a converged internet protocol (IP) standards-based communications network, optimizing reliable connectivity paths
  • IP67 certified to support installation in production facilities or on existing outdoor infrastructure
  • Backward compatible to support network expansion and modernization
  • Edge-compute ready
  • Optional internal backup battery allows the device to work without external power for several hours

About Hitachi Energy

Hitachi Energy is a global technology leader that is advancing a sustainable energy future for all. We serve customers in the utility, industry and infrastructure sectors with innovative solutions and services across the value chain. Together with customers and partners, we pioneer technologies and enable the digital transformation required to accelerate the energy transition towards a carbon-neutral future. We are advancing the world's energy system to become more sustainable, flexible and secure whilst balancing social, environmental and economic value. Hitachi Energy has a proven track record and unparalleled installed base in more than 140 countries. We integrate more than 150 GW of HVDC links into the power system, helping our customers enable more wind and solar. Headquartered in Switzerland, we employ more than 40,000 people in 90 countries and generate business volumes of over $10 billion USD. 

https://www.hitachienergy.com

https://www.linkedin.com/company/hitachienergy

https://twitter.com/HitachiEnergy

About Hitachi, Ltd.

Hitachi drives Social Innovation Business, creating a sustainable society through the use of data and technology. We solve customers' and society's challenges with Lumada solutions leveraging IT, OT (Operational Technology) and products. Hitachi operates under the 3 business sectors of “Digital Systems & Services” – supporting our customers’ digital transformation; “Green Energy & Mobility” – contributing to a decarbonized society through energy and railway systems, and “Connective Industries” – connecting products through digital technology to provide solutions in various industries. Driven by Digital, Green, and Innovation, we aim for growth through co-creation with our customers. The company’s revenues as 3 sectors for fiscal year 2023 (ended March 31, 2024) totaled 8,564.3 billion yen, with 573 consolidated subsidiaries and approximately 270,000 employees worldwide. For more information on Hitachi, please visit the company's website at https://www.hitachi.com.

Contacts

Photo of
Media Relations

Hitachi Energy

Alle Nachrichten