Maintenance release of LHMI firmware for Relion® 670/650 series
Product Release | Västerås, Sweden | 26.11.2019 | 2 min read
Product Release | Västerås, Sweden | 26.11.2019 | 2 min read
RELEASE NOTE 1MRG037497 – NOVEMBER 22, 2019
Please read all about the system and security related updates in the release note.
We recommend users who have faced issues mentioned in this release note to update to this release.
Updating to the new LHMI firmware does not require any changes in the installed IED Connectivity Packages for Relion 670/650 series.
All new and existing orders on 670 series versions 2.0, 2.1, 2.2 and 650 series 2.1, 2.2 will be delivered with the updated LHMI firmware.
Procedure for ordering the firmware update:
The LHMI is updated using Field Service Tool (FST). Please follow the below procedure for ordering the FST.
Please note that it is extremely important that you report back to us via SE-mets.submit@abb.com when the update of the concerned LHMI/IED has been completed. This information is needed to keep our product register updated and to ensure right information to the right local ABB units in the future.
Kind regards,
Joseph Menezes, Global Product Manager