Choose your region and language

Go

Menu

Unique collaboration sees Hitachi Energy decarbonize construction site in Sweden

Press Release | Vasteras, Sweden | 19.03.2024 | 3 min read

Magnus Persson, CEO Skanska Sweden , Tobias Hansson, Country Managing Director,  Hitachi Energy Sweden, Richard Berkling, CEO PowerCell Group, Viktor Allgurén, Head of Innovation Port of Gothenburg, Niklas Wahlberg, VP Partnership and System Solutions, Volvo Group,  Linda Sahlén, Project manager, Linde Gas and Kenneth Andersen, Manager Mobile Energy at Skagerak Energi. The picture is taken in a safe area with no activity.

  • Hitachi Energy’s HyFlex™ hydrogen-powered generator supplied clean power to an on-site charging station.
  • The hydrogen generator was used on a construction site in collaboration with PowerCell Group, Skanska, Volvo,  Port of Gothenburg, Linde Gas, and Skagerak Energi

The innovative hydrogen project at Skanska's construction site in the Port of Gothenburg is the first demonstration of HyFlex at a customer field location. For two weeks, the unit ran on green hydrogen supplied by Linde Gas to generate clean electricity for an on-site charging station. The station supplies power to a Volvo electric excavator used for civil work on the site.

The collaboration represents a milestone in the electrification and decarbonization of construction sites, with each party contributing their technology expertise.

Hitachi Energy’s HyFlex is designed to serve as a clean alternative to diesel generators, which are commonly used on construction sites that don’t have access to grid power. It is completely emission-free during operation, producing AC power, usable heat, and water.1

As a highly scalable and portable plug-and-play solution – the HyFlex unit can be transported and used immediately. It includes fuel cell modules, power electronics, cooling, auxiliaries, and an intelligent control system. Hitachi Energy’s technology partner, PowerCell Group, has provided the power modules and know-how in fuel cell integration. The generator is enclosed in an easily transportable container creating minimal noise output during operation.

“This is a great example of the importance and power of collaboration, when industry leaders come together to accelerate the energy transition, says Tobias Hansson, Country Managing Director, Hitachi Energy in Sweden. “The HyFlex installation at Skanska´s construction site in the Port of Gothenburg successfully demonstrates how this hydrogen-powered fuel cell technology can serve as a clean a reliable alternative to diesel generators” he added.

" Fossil free construction sites is an important part of the construction sector´s strive for net zero emissions. In order to succeed with the climate transition, cooperation with other sectors is crucial. This test was made possible by the great teamwork with Hitachi Energy, Volvo and other partners, says Magnus Persson, CEO Skanska Sverige AB. 

"There is no one key that will unlock our decarbonization journey. At Volvo Group, we strongly believe that different solutions are needed if we are to accelerate our customers’ transition towards fossil free sites. This project is testament to the power of partnership and a flexible decarbonization approach that sees different technologies, and companies, working towards a shared goal. Together, we make the most sustainable choice today so that every step we take moves us closer towards net zero”​, says Niklas Wahlberg, VP Partnership and System Solutions, Volvo Group.

Hitachi Energy is developing multiple modular variants of the HyFlex generator to suit the needs of various markets and applications, including remote construction sites, mines, large-scale events, data centers, and others. The unit deployed at the Port of Gothenburg site is a scaled-down version of the commercial offering which will be released for sale in the near future.