Hitachi Energy, LKAB and Scania are joining forces to accelerate the electrification of mining operations with autonomous pantograph-down charging solution for electric trucks in an underground mine in Malmberget, Sweden. The project combines LKAB’s experience in mining operations, Scania’s electric heavy-duty vehicles and Hitachi Energy’s expertise in electrification and charging infrastructure to integrate electric transport and automated high-power charging into day-to-day mining operations.
Electrifying heavy-duty transport is an important part of reducing mining’s reliance on fossil fuels.
Hitachi Energy’s Grid-eMotion® Fleet charging solution has been configured for the underground mining environment, with a fixed overhead pantograph that automatically connects to the truck for charging. Installed 1,250 meters below ground at LKAB’s Malmberget mine, the system will deliver more than 400 kW of charging power, enabling trucks to recharge within minutes during operational stops. With no manual connection or additional ground space required, charging can be integrated directly into the mining operation.