Choose your region and language

Go

Menu

Thyristor controlled series compensation

Hitachi Energy's Thyristor Controlled Series Compensation (TCSC) provides an advanced solution to future grid challenges. TCSC is a grid enhancing technology (GET) that improves active power transfer while mitigating the risk of sub-synchronous resonance (SSR). It enables dynamic power flow control (PFC) and facilitates active power oscillation damping (POD). The system also supports renewable integration without introducing sub-synchronous control interaction (SSCI) risks, offering effective congestion management and serving as a flexible alternative to traditional infrastructure expansion. By implementing TCSC, utilities can optimize grid performance amid evolving conditions, ensuring both resilience and operational efficiency in response to the changing demands of the energy sector. 

Hitachi Energy commissioned its first TCSC installation in 1999. With more than 25 years of experience and the largest installed base worldwide, we have an unmatched operational knowledge in applying TCSC for complex and high-impact transmission projects.

Product image for: Thyristor controlled series compensation

Applications

 

  • Sub-synchronous resonance (SSR) mitigation
  • Sub-synchronous control interaction (SSCI)
  • Dynamic power flow control (PFC) 
  • Power oscillation damping (POD)

Design overview

Like traditional Fixed Series Capacitors, all the main equipment of the TCSC is installed on an insulated steel platform. The system comprises a thyristor-controlled inductor connected in parallel with the capacitor bank. Overvoltage protection is through Metal Oxide Varistor (MOV). Control and protection systems are located at ground level and interfaced through fiber optic links to ensure high-speed, reliable operation.

How it works

Hitachi Energy's patented firing control algorithm dynamically adjusts the impedance of transmission lines using advanced power electronic devices. Notably, this algorithm provides inherent immunity to the entire sub synchronous resonance (SSR) frequencies, distinguishing it from other mitigation methods such as SSR filter solutions.

Key Benefits of TCSC

Affordability

TCSC unlocks higher usable transmission capacity. This reduces the need for new transmission corridors and lowers investment costs and losses — directly improving the cost of delivering electricity.

Timeliness

Through SSR mitigation, power oscillation damping and dynamic power flow control, TCSC strengthens system stability and protects critical generation assets.

Sustainability

TCSC supports large-scale integration of wind and other renewable sources — accelerating the transition to a low-carbon grid.

Advantages of TCSC compared to SSR filter solution

  • TCSC is controlled to present an inductive impedance at sub‑synchronous frequencies, thereby preventing or damping SSR. By contrast, an SSR filter does not remove the resonance mechanism but instead reduces its effects by attenuating sub‑synchronous components.
  • Normally, SSR filters are tuned for a particular frequency range, so any change in the network may require filter retuning. TCSC is a robust solution for the entire SSR frequency band, so changes in the network condition have no impact.
  • For TCSC, degree can be adjusted within the design limit whereas compensation degree is fixed in SSR filter.
  • TCSC has a smaller footprint compared to the filter solution due to advanced power electronics.
  • TCSC has lower losses as compared to SSR filter solution
  • Power flow control is an additional feature of a TCSC that is not possible in SSR filter.
  • Power oscillation damping is possible with TCSC, though not with SSR filter.

As we look toward the future grid, Thyristor Controlled Series Compensation (TCSC) stands out as a versatile solution addressing multiple challenges. This cutting-edge technology not only streamlines renewable integration by eliminating the risk of Sub-Synchronous Control Interaction (SSCI), but also alleviates grid congestion and actively dampens power oscillations. TCSC empowers utilities to build a more resilient, efficient, and sustainable transmission network.

Nandagopal R.
Global Product Specialist, Series Compensation 

TCSC in Social Media

Powering the Energy Transition in America

Hitachi Energy has been awarded a prestigious contract in Peru by ALUPAR to deliver four Thyristor-Controlled Series Capacitors (TCSCs) for a first-of-its-kind Power Flow Control (PFC) application in the region.

Series Compensation Solutions - Brochure

Maximize transmission capacity.
Enhance grid resilience.

Frequently Asked Questions

TCSC is primarily installed in transmission corridors where enhanced power transfer capability is required to meet energy demand, particularly in networks that are susceptible to Sub-Synchronous Resonance (SSR) or Sub-Synchronous Control Interaction (SSCI).

Yes, TCSC offers inherent immunity to sub-synchronous resonance (SSR) and sub-synchronous control interaction (SSCI). At sub-harmonic frequencies, the power system perceives the TCSC as an inductor, hence any variations in the grid condition do not affect the performance of TCSC.

TCSC (Thyristor Controlled Series Capacitor) prevents control interactions between wind turbine converters and series-compensated transmission lines, thereby reducing the risk of Sub-Synchronous Control Interaction (SSCI), a critical issue in large-scale wind farm integration. 

As renewable integration can lead to grid congestion, TCSC's dynamic impedance controllability provides an effective solution for alleviating such congestion.