Hitachi Energy is at the forefront of the energy transition by collaborating with customers and partners to support worldwide efforts to reduce the impact of greenhouse gases such as sulfur hexafluoride (SF6).
SF6 has been the norm in the industry for decades, but that will soon change. Even though SF6 has excellent insulation capabilities, it has a high Global Warming Potential (GWP), and its life-cycle management requires careful handling.
As the first big step forward, we launched our EconiQ® high-voltage portfolio in 2021 to phase out SF6 and enable the industry to transition to eco-efficient solutions. Since then, EconiQ has achieved multiple world-firsts in SF6-free high-voltage technologies and is becoming widely adopted across continents.
A new era of EconiQ is coming. In CIGRE Session 2024, we have unveiled two truly iconic EconiQ additions that demonstrate how the scalability of our technology plays a fundamental role in the effective elimination of SF6.
Join us on our journey to an SF6-free energy future!
EconiQ high-voltage portfolio roadmap
World’s first 550 kV eco-efficient circuit breaker
Hitachi Energy’s latest sustainable innovation that scales eco-efficient technology to the highest voltage ratings and marks a significant milestone in the journey to phase out SF6 from the grid.
EconiQ 420 kV circuit breaker
This breakthrough technology is a significant milestone in the industry to transmit large amounts of electricity over long distances while eliminating significant volumes of SF6.
EconiQ Live Tank Circuit Breaker 420 kV
The latest addition to Hitachi Energy’s EconiQ high-voltage line that is as reliable ast he conventional solution and operates with an eco-efficient gas mixture that significantly reduces the environmental impact.
Discover Hitachi Energy’s EconiQ milestones
Book a free consultation
Take action today to ensure smooth operation tomorrow
Book your free consultation today