Selecciona tu región e idioma

Menú

The opportunity

Hitachi Energy is seeking a Site Quality Manager (SQM). The role will be based in the field at the project location.  Role requires relocation to new project site upon completion. This role is responsible for planning, organizing, leading, and monitoring all Quality work during site execution to ensure we satisfy customer expectations. This includes works undertaken internally in addition to the work performed by our partners as required for the project. The SQM reports functionally to the Quality & CI Manager for Site Quality. During site execution the Site Quality Specialist reports operationally to the Site Manager and dotted to the PQM. The role will be based in the field at the project location - Current project location is Peterhead

Please note we are unable to provide visa sponsorship on this position.

 

How you’ll make an impact 

  • Review contractual and local requirements applicable to site quality. Review lessons learnt from previous projects and relevant project plans (e.g., SQP, SMP).
  • Review Contractor Quality Plans to ensure alignment with the Project Quality Plans and the customer requirements. Based on reviews and discussion with stakeholders identify and follow up risks and mitigations to ensure we fulfill site quality expectations.
  • Set up and educate site personnel in the quality management system including the completion system at site and ensure it is compliant with any regulatory and PG requirements as well as any applicable codes & standards.
  • Provide Quality Induction training to the site personnel. Execute and follows up the Quality Plans, master test plan and completion system status for site activities as required.
  • Review quality documentations for correctness and completeness prior approval (e.g., test certificates, checklist, etc.). Ensure that the quality control plans (ITP, ITR etc.) and any erection documentation (isometrics, procedures, etc.) provided by HVDC are effectively communicated to the site management team and the contractors.
  • Ensure that Quality Control processes are fully implemented and continuously monitored. Ensure that inspection / testing during Civil, Mechanical & Electrical erection and Commissioning are conducted, documented, checked, and validated as per the quality control system.
  • Organize and supervise acceptance testing and/or approval by customers, third parties and governmental authorities whenever required at site. Ensure that the completion system, deviation, NCR (Non-Conformance Report) System, CCRP system and any other Quality tools are fully deployed at site and that the users are adequately trained.
  • Ensure that all testing and measurement equipment used at site are listed and calibrated and that the associated calibration certificates are available. Follow up completion system at site having an overview of status regarding inspections, certifications and all outstanding works including punch list.
  • Provide Quality related site KPIs to the stakeholders whenever required. Coordinate, follow-up, and lead site inspections and support the management of punch-out items. Provide Quality inputs to the site management to support on-time and in-budget execution of the project.
  • Perform site quality inspection of goods coming to site and report any deviations according to the project regulations. Follows up that handling, storage of delivered material and equipment are in accordance with the manufacture's guidelines and the SQP.
  • Ensure that the ITP/ITR are applied by the sub-contractor and its subcontractors including the compliance with the Hold points and Witness points. Ensure site quality documentation is generated, distributed, updated, and archived in accordance with the Management system and completion system requirements. Deploy Site Quality audit program (including contractor audits and internal audits).
  • Participate in internal and contractor quality audits as per the Site Quality audit program. Assist and coordinate any planned external site related audits. Monitor contractor compliance with Quality requirements and implement corrective actions whenever required.
  • Follow up the adherence and governance of the quality management system at site. Support in identifying lessons learnt and contribute with input to the ToE process.

Your background 

  •  Technical / engineering / quality management education – minimum bachelor’s degree. 
  • 5+ year construction quality site experience or in operations 
  • Power or energy industry experience 
  • Track record and proven capability in Change Management, managing internal project/program in large 
  • and complex organization 
  • ISO0991 knowledge, L6S Belt, MS Office suite
  • Ability to travel

Ubicación Glasgow, Scotland, United Kingdom
Tipo de empleo Full time
Modalidad de trabajo On-Site
Experiencia Experienced
Función laboral Quality Management
Contrato Regular
Fecha de publicación 2026-04-22
Número de referencia R0126310

Sobre Hitachi Energy

Hitachi Energy es líder mundial en electrificación, impulsando la era de la electricidad para satisfacer las demandas energéticas actuales y las de los próximos 25 años. Como división energética del Grupo Hitachi, más de tres mil millones de personas dependen de nuestras tecnologías pioneras y de misión crítica para su vida cotidiana.

Con más de un siglo de innovación, estamos abordando el desafío energético más urgente de nuestro tiempo: impulsar la evolución del sistema energético mundial para garantizar una energía abundante, segura, asequible y sostenible para la generación actual y las futuras.

Con una base instalada sin igual en más de 140 países, somos el socio del ecosistema de la red eléctrica en los sectores de servicios públicos, industria, centros de datos y transporte. Con sede en Suiza, contamos con más de 56 000 empleados en 60 países y generamos ingresos de alrededor de 20 000 millones de dólares estadounidenses.