Selecciona tu región e idioma

Menú

The opportunity

Responsible for Configuration of IED’s used in EHV Substations, Development of HMI’s using vendor specific tools and testing of CRP and SAS of EHV substations (above 132kV Voltage level). Ensure that the Substation Automation Projects delivered by HEIL are configured as per the project requirements and tested, put into service on time, meeting highest HEIL quality and OHS standards. Meet or exceed the customer expectations in testing & configuration of IED in line with project requirements.

How you’ll make an impact

  • As a testing and configuration engineer, carrying out the configuration of IED’s, development of HMI’s in line with project requirements and testing of Control and relay panels, Substation automation system delivered and actively contribute in the testing team of Grid Automation Systems.

  • Execute the project IED’s configurations and testing safely following all safety standards of HEIL as well as customer. Reports Hazards, Near Misses at working location back to office for records and further improvement.

  • Ensure that customer relations are managed in an optimal way. Carryout the Configurations of IED’s and testing the Control, Protection and SAS panels as per the documented process description and checklists. Continuous interactions with testing Lead and expert help to carry out the testing works effectively.

  • Report the Configuration and testing project status testing progress & testing plan to testing Lead. Ensure efficient use of the testing assets like Test kits, Tools etc.

  • Ensures project information of any project is fully taken from testing lead  and get all IED’s fully configured and tested in line with customer approved drawings and  ready for the project specific testing activities before offering the projects to customer during FAT.

  • Handing over the marked-up drawings to engineering for preparing the As-build drawing and onward submission to customer to close the project.

  • Handover the final testing backup CD's, Micro SCADA system backup, IET workplace backup and other backup as per the checklist to lead.

  • Actively and regularly (Compulsory for every project) provides feedback to Engineering Project Management, manufacturing and quality in way that ensures re-usage of experience. Follow the key process like  Test procedures ,Time sheets and  STAART Metings.

  • Ensure the installed base numerical relays are maintained with minimum revisions by continuosly updating the older revisions.

  • Ensure the usage of the latest tools and latest software versions during  project IED configurations and testing.

  • Continous learning & acquiring expertise in various protection schemes and Automation system to achieve the higher  growth in  ‘learning curve’.

  • Responsible to ensure compliance with applicable external and internal regulations, procedures, and guidelines.

  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background

  • Should be a graduate in BE Electrical engineering and should have a minimum of 3 years of experience in testing and commissioning of control and relay panels in projects above 132kV Voltage levels.

  • Should have good knowledge on Power system.

  • Should have hands on experience with 3 Phase injection test kits like Omicron, Doble, Megger, Ponova etc…

  • Should have good knowledge on understanding the schematics of control and relay Panels, primary equipment interlocks.

  • Should be ready for frequent travels all over India and overseas wherever assigned for at least next 5 years.

  • Should have e good knowledge on configuration of HEIL IED’s and competitors IED’s in line with project requirements

  • Should have a minimum of 3 years of experience in commissioning of SAS with IEC61850 standards, IEC101, IEC104, OPC and Modbus protocols.

  • Should have good knowledge on communication protocols listed above.

  • Should have good knowledge on IEC61850 standards, Ethernet, Serial communications.

  • Should have good knowledge on communication protocols such as Modbus, DNP 3.0, IEC 101, IEC 104, OPC,

  • Should have competency on networking, configuration of managed Ethernet switches.

  • Should have hands on experience on Protocol analyzers like IEC browser and network analyzer tools like wire sharks

  • Project drawings & Documents from Test Lead. Project IED configurations plan and testing of panels progress reports on daily basis.

  • Clear with min MOM points during customer FAT. Handing over of project backups once testing is closed.

  • Proficiency in both spoken & written English language is required.

Ubicación Bengaluru, Karnataka, India
Tipo de empleo Full time
Modalidad de trabajo On-Site
Experiencia Experienced
Función laboral Engineering & Science
Contrato Regular
Fecha de publicación 2026-05-23
Número de referencia R0131014

Sobre Hitachi Energy

Hitachi Energy es líder mundial en electrificación, impulsando la era de la electricidad para satisfacer las demandas energéticas actuales y las de los próximos 25 años. Como división energética del Grupo Hitachi, más de tres mil millones de personas dependen de nuestras tecnologías pioneras y de misión crítica para su vida cotidiana.

Con más de un siglo de innovación, estamos abordando el desafío energético más urgente de nuestro tiempo: impulsar la evolución del sistema energético mundial para garantizar una energía abundante, segura, asequible y sostenible para la generación actual y las futuras.

Con una base instalada sin igual en más de 140 países, somos el socio del ecosistema de la red eléctrica en los sectores de servicios públicos, industria, centros de datos y transporte. Con sede en Suiza, contamos con más de 56 000 empleados en 60 países y generamos ingresos de alrededor de 20 000 millones de dólares estadounidenses.