Selecciona tu región e idioma

Menú

As a commissioning engineer, carrying out the testing & Commissioning of Control and relay panels, 
Substation automation system delivered in various locations within and outside India and actively 
contribute in the Zonal Service Management team of Grid Automation Systems. 

Execute the project commissioning safely following all safety standards of ABB as well as customer. 
Reports Hazards, Near Misses at working location back to office for records and further 
improvement. 

Ensure that customer relations are managed in an optimal way. 

Carryout the commissioning as per the documented process description and checklists. Continuous 
interactions with Zonal service manager and expert helpline to carry out the site works effectively. 
Clear MOM to be signed off with customer before leaving the site. 

Report the Site progress & Site plan to Zonal Service Manager. Ensure efficient use of the 
commissioning assets like Test kits, Tools, Ferule machines etc. 

Ensures project information of any project is fully taken from zonal service manager and get fully 
ready for the project specific site activities before leaving to site. 

Handing over the marked-up drawings to engineering for preparing the As-build drawing and 
onward submission to customer to close the project. 

Handover the final site backup CD's, MicroSCADA system backup, IET workplace backup and other 
backup as per the checklist to ZSM. 

Actively and regularly (Compulsory for every project) provides feedback to Testing, Project 
Management, Engineering and Sales in way that ensures re-usage of experience.  

Follow the key process like Time sheets, compulsory entry of sale ordernumber in TI and return with 
clear MOM as per standard format. 

Ubicación Remote - Karnataka, India
Tipo de empleo Full time
Modalidad de trabajo On-Site
Experiencia Entry Level
Función laboral Engineering & Science
Contrato Regular
Fecha de publicación 2026-06-16
Número de referencia R0126722

Sobre Hitachi Energy

Hitachi Energy es líder mundial en electrificación, impulsando la era de la electricidad para satisfacer las demandas energéticas actuales y las de los próximos 25 años. Como división energética del Grupo Hitachi, más de tres mil millones de personas dependen de nuestras tecnologías pioneras y de misión crítica para su vida cotidiana.

Con más de un siglo de innovación, estamos abordando el desafío energético más urgente de nuestro tiempo: impulsar la evolución del sistema energético mundial para garantizar una energía abundante, segura, asequible y sostenible para la generación actual y las futuras.

Con una base instalada sin igual en más de 140 países, somos el socio del ecosistema de la red eléctrica en los sectores de servicios públicos, industria, centros de datos y transporte. Con sede en Suiza, contamos con más de 56 000 empleados en 60 países y generamos ingresos de alrededor de 20 000 millones de dólares estadounidenses.