Selecciona tu región e idioma

Menú

The opportunity:

Hitachi Energy is a global technology leader that is advancing a sustainable energy future for all. We serve customers in the utility, industry and infrastructure sectors with innovative solutions and services across the value chain. Together with customers and partners, we pioneer technologies and enable the digital transformation required to accelerate the energy transition towards a carbon-neutral future. We are advancing the world’s energy system to become more sustainable, flexible, and secure whilst balancing social, environmental, and economic values.

Modular Advanced Control for HVDC (MACH™), is the brain in HVDC transmission systems. This system is designed to run 24/7 for thirty years or more, allowing the HVDC system to be controlled and protected in the most reliable way throughout its lifetime.
The system consists of Control & Protection Main Computers, Station Control and Monitoring servers, Operator Workstations, Digital Signal Processing units, Input / Output systems and Valve Control Units.

How you’ll make an impact:

  • To define verification scope, areas, considering the boundaries and limits, performance & parameters, functional & non-functional requirements. Write Test Plan / Test Specifications, Test Cases / Scenarios for verifying the functionalities of the Control System, for product and sub-system level verification, for the product and sub-system requirements / parameters.

  • To create Test Environment with the components of MACH Control System in the Test Lab Facility, with Computers, Servers, Input - Output Boards and Simulation Environments, for test developments and execution. Execution of Test Cases, for various software and hardware releases using the developed test cases in the test lab.

  • Report on the test execution details to the development team for further actions. Capturing the Key Performance Indicators (KPIs), report & use for further improvements. Maintain the test environment with updated software and hardware for current and future use.

  • Follow the processes for product and sub-system verification, within the overall MACH control system product development & release, for planning, execution, reviews & reporting. Adhere to the defined & approved process, in full, all the time.

  • To Focus on automation, continuously, for efficiency and quality improvements. Define & implement. Continuously improve the test scenarios, execution and reporting, for efficiency and effectiveness.

  • To Support the management for strategy and planning, for the future verification needs. Deliver value with Quality, On-Time.

  • Responsible for ensuring compliance with applicable external and internal regulations, procedures, and guidelines.

  • Living Hitachi Energy’s core values safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your Background:

  • Required Graduate or master’s degree in engineering (Electrical & Electronics, Electronics and communication, Instrumentation & Control) with more than 5 years of proven experience in product verification, with exposure to the complete testing life cycle.

  • Exposure / experience working with verification of power systems or similar products, is a huge plus. Experience / exposure, working with control & protection, events & alarms, time synchronization, HMI, communication protocols such as IEC61850, Modbus etc.

  • Hands-on experience in writing test plans / test specifications, test cases, test reports. Experience in working with test management tools such as TFS or similar. Experience with Test Automation implementation (Python/ other tools).

  • ISTQB or similar certification, is preferred. Experience with processes such as Agile / Scrum.

  • Required Strong communication - both verbal & written, and collaboration skills, Self-driven, Good intercultural sensitivity. Coaching & mentoring skills.
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
Fecha de publicación 2026-09-03
Número de referencia R0142664

Sobre Hitachi Energy

Hitachi Energy es líder mundial en electrificación, impulsando la era de la electricidad para satisfacer las demandas energéticas actuales y las de los próximos 25 años. Como división energética del Grupo Hitachi, más de tres mil millones de personas dependen de nuestras tecnologías pioneras y de misión crítica para su vida cotidiana.

Con más de un siglo de innovación, estamos abordando el desafío energético más urgente de nuestro tiempo: impulsar la evolución del sistema energético mundial para garantizar una energía abundante, segura, asequible y sostenible para la generación actual y las futuras.

Con una base instalada sin igual en más de 140 países, somos el socio del ecosistema de la red eléctrica en los sectores de servicios públicos, industria, centros de datos y transporte. Con sede en Suiza, contamos con más de 56 000 empleados en 60 países y generamos ingresos de alrededor de 20 000 millones de dólares estadounidenses.