Selecciona tu región e idioma

Menú

Mission Statement Perform Installation & Commissioning site activities for GIS- HV Services in accordance with the time schedule, quality standards and safety requirements. Manage On site activities by ensuring availability of material, equipment’s & resources as per the contract specifications.

Your Responsibility

  • Installation & Commissioning: Understanding the specification and completing the installation & Commissioning site activities according to the contractual requirement & time schedule.
  • On Site Service: Ensure availability of necessary material, equipment & manpower at site by coordinating with the respective stakeholders.
  • Manage site activities as per the time schedule until completion of the project and inform Field service project Manager or service manager for assistance required for additional resources / material.
  • The GIS-Supervisor is responsible for the installation work entrusted to him being carried in perfect technical order. He carries out installation and maintenance work independently. He instructs, supervises, and controls the installation personnel reporting to him at site. He is responsible for ensuring compliance with the installation requirements and instructions.
  • He ensures necessary accident prevention measures are observed; specifically, he abides by the guidelines for work on live system components.
  • He supervises the adherence to the working hours, signs the mom, weekly reports & timesheets and is responsible for forwarding these on.
  • The GIS Supervisor ensures that the stipulated deadlines are met, i.e., he is responsible for detailed installation planning on-site to enable bottlenecks to be identified in good time, to formulate proposals for achieving targets and implementing appropriate measures. Testing perform testing for Installed & Commissioned products and provide input to the design team for any modification.
  • Quality Control: Verifies the application of quality control plan during installation activities and that the sub contractors are using the safety equipments as per the requirement .
  • Documentation: Coordinates with the customer on documentation required and safety coordination. Information: Inform respective stakeholders on the progress of Installation & Commissioning activities and provide input to the quality team for any non conformance.
  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business .

Your Background

  • Qualification & Experience: Diploma (Mechanical / Electrical): 5 – 7 Years experience.
  • BE (Mechanical / Electrical): 3 – 4 Years experience.
  • Information inform respective stakeholders on the progress of Installation & Commissioning activities and provide input to the quality team for any non conformance.
  • Proficiency in both spoken & written English language is required .

Ubicación Maneja, Gujarat, India
Tipo de empleo Full time
Modalidad de trabajo On-Site
Experiencia Experienced
Función laboral Engineering & Science
Contrato Regular
Fecha de publicación 2026-09-07
Número de referencia R0141278

Sobre Hitachi Energy

Hitachi Energy es líder mundial en electrificación, impulsando la era de la electricidad para satisfacer las demandas energéticas actuales y las de los próximos 25 años. Como división energética del Grupo Hitachi, más de tres mil millones de personas dependen de nuestras tecnologías pioneras y de misión crítica para su vida cotidiana.

Con más de un siglo de innovación, estamos abordando el desafío energético más urgente de nuestro tiempo: impulsar la evolución del sistema energético mundial para garantizar una energía abundante, segura, asequible y sostenible para la generación actual y las futuras.

Con una base instalada sin igual en más de 140 países, somos el socio del ecosistema de la red eléctrica en los sectores de servicios públicos, industria, centros de datos y transporte. Con sede en Suiza, contamos con más de 56 000 empleados en 60 países y generamos ingresos de alrededor de 20 000 millones de dólares estadounidenses.