Selecciona tu región e idioma

Menú

The Customer Training Coordinator is responsible for: 

 

  • Coordinate the processes for Power Quality Solutions Customer Trainings. In this role, the training coordinator will be responsible to organize the demands related to customer trainings, both during tender stage and during project execution. 

  • During the tender stage, the Customer Training Coordinator is responsible to define the training program and calculate the costs to execute it. The training program must be based on the customer requirements and specifications.  

  • During the execution, the Training Coordinator is responsible to make sure that all the deadlines are accomplished, and the trainings are planned well in advance, including material preparation, updates, logistics and resources.  

  • The Customer Training Coordinator is responsible to make sure that the necessary alignment is done with the different departments, being responsible to organize and coordinate meetings and processes. 

  • This role is part of the Engineering team and will interact cross functionally in the organization. The Customer Training Coordinator will be working closely with different departments and units across the globe since many of the trainings are prepared on demand for them. 

  • Update Training documentation, develop and standardize the training material and make it accessible to the organization. 

Ubicación Chennai, Tamil Nadu, India
Tipo de empleo Full time
Modalidad de trabajo On-Site
Experiencia Experienced
Función laboral Customer Service & Contact Center Operations
Contrato Regular
Fecha de publicación 2026-10-21
Número de referencia R0141266

Sobre Hitachi Energy

Hitachi Energy es líder mundial en electrificación, impulsando la era de la electricidad para satisfacer las demandas energéticas actuales y las de los próximos 25 años. Como división energética del Grupo Hitachi, más de tres mil millones de personas dependen de nuestras tecnologías pioneras y de misión crítica para su vida cotidiana.

Con más de un siglo de innovación, estamos abordando el desafío energético más urgente de nuestro tiempo: impulsar la evolución del sistema energético mundial para garantizar una energía abundante, segura, asequible y sostenible para la generación actual y las futuras.

Con una base instalada sin igual en más de 140 países, somos el socio del ecosistema de la red eléctrica en los sectores de servicios públicos, industria, centros de datos y transporte. Con sede en Suiza, contamos con más de 56 000 empleados en 60 países y generamos ingresos de alrededor de 20 000 millones de dólares estadounidenses.