Selecciona tu región e idioma

Menú

Business Information:

Our Indian Operations Centre (INOPC) is a competence center with around 2600+ skilled engineers who focus on tendering, engineering, planning, procurement, functional system testing, installation supervision, and commissioning. Over the last decade, INOPC has evolved to become the largest engineering hub serving more than 40 countries across different energy sectors. The team caters to the four business units—Transformers, Grid Integration, Grid Automation, High Voltage and has successfully executed engineering and commissioning for projects in more than 80 countries.

 

Main Accountabilities:

Hitachi Energy is the world leader in Power Quality Solution – PQS (former– FACTS) (Flexible AC Transmission System) technology and offers a full PQS portfolio with in-house manufacturing of key components.  Hitachi Energy was the first to introduce PQS to the power industry and has delivered PQS equipment for more than 50 years. Today Hitachi Energy is the recognized world leader with more than 50 percent of the global market share and more than 700+ installed bases. Hitachi Energy has a number of solutions that enhance the security, capacity and flexibility of power transmission systems. These solutions enable power grid owners to increase existing transmission network capacity while maintaining or improving the operating margins necessary for grid stability.  Hitachi Energy has the full FACTS portfolio and in-house manufacturing of key components

Hitachi Energy uses a very high-end system for its control, protection and monitoring. This system is called as MACH. This computerized system is built with the state-of-the-art electronics, microprocessors and digital signal processors, connected by high performance industry standard busses and fiber optic communication links.

Hitachi Energy PQS Electrical Engineering (EE) is responsible for the designing of MACH hardware control and Protection system, IED based Control & Protection system, Configuration & testing of Protection system, Auxiliary AC & DC system design including MV/LV Switch boards, Battery systems, UPS, Voltage stabilizers, LV Cable sizing and estimation & Interlocking systems

 

Roles and responsibilities:

 

As the PQS Electrical engineering (Secondary Design) is being continuously involved with great deal of Electrical, Domain expertise is required. Thus, the job description is as below.

  • Execute project within budget by meeting all KPI's (Quality, OTD, Efficiency, Budget)
  • Design & execute the project in line with customer specification / FACTS standard/Global standards Viz IEC, ANSI, IEEE etc.
  • Tender execution as per customer/FACTS requirement
  • Preparation of MACH based control and protection system cubicle design
  • Preparation of IED based control and protection system cubicle design
  • Preparation of FACTS Plant design drawings (Secondary)
  • Designing and estimation of Aux. AC & DC power requirements.
  • Designing of LV, MV Switch boards including battery systems, UPS and Voltage stabilizers
  • Estimation & Sizing of LV Aux. power, control cables, communication cables & Indication cables
  • Purchasing of cubicles, cables, Junction boxes, AC & DC switch boards, MV Switchgear, Battery system, UPS & Voltage stabilizers etc.
  • Co-ordination with other departments (Mech. / Control / System Design/Commissioning)
  • Validation of the time schedule (EE Dept.) for a project
  • Review and coordination with vendor/supplier drawings for Electrical deliverables including primary equipment
  • Evaluation of sub-supplier and selection as per project requirement
  • Supporting for configuration & testing of protection system
  • Involving in customer FAT, site installation and commissioning support
  • Involving in development and supporting activities for continuous process improvements
  • Preparation of As Built Drawings
  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business

 

Your background:

  • Should be a   BE in Electrical Engineering
  • 6 - 10 years of experience in Substation secondary/EPC design or project execution or HVDC control & protection hardware design
  • Strong experience and substation /EPC project execution or HVDC secondary project execution & Strong Experience in Control and Protection cubicle design
  • Experience in Detailed Design of plant Engineering & Works independently, applying established local & global standards
  • Experience in Electrical Grid Industry (Switchyard equipment) & Experience in E3 or Similar design tool handling
  • Experience in ETAP software for auxiliary system design, load flow analysis and short circuit study & Experience in Cable engineering
  • Team contributor using in-depth knowledge in a specific area to execute complex or specialized projects / challenges often thinking independently to challenge traditional solutions.
  • Comprehensive knowledge of related disciplines in the organization
  • Excellent English speaker, good communication skills & Dynamic and Proactive, willing to take the challenges and grow in the organization
  • Team player, ready to play the role across the different departments/countries
  • High level of ownership & accountability
  • Strong communication and interpersonal skills, with the ability to collaborate effectively with cross-functional teams
  • Attention to detail and a commitment to delivering high-quality digital solutions.
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
Fecha de publicación 2026-10-21
Número de referencia R0146338

Sobre Hitachi Energy

Hitachi Energy es líder mundial en electrificación, impulsando la era de la electricidad para satisfacer las demandas energéticas actuales y las de los próximos 25 años. Como división energética del Grupo Hitachi, más de tres mil millones de personas dependen de nuestras tecnologías pioneras y de misión crítica para su vida cotidiana.

Con más de un siglo de innovación, estamos abordando el desafío energético más urgente de nuestro tiempo: impulsar la evolución del sistema energético mundial para garantizar una energía abundante, segura, asequible y sostenible para la generación actual y las futuras.

Con una base instalada sin igual en más de 140 países, somos el socio del ecosistema de la red eléctrica en los sectores de servicios públicos, industria, centros de datos y transporte. Con sede en Suiza, contamos con más de 56 000 empleados en 60 países y generamos ingresos de alrededor de 20 000 millones de dólares estadounidenses.