Selecciona tu región e idioma

Menú

The Data Center and the Grid: The Flexible relationship driven by AI and managed by Automation

Blog Post | 02.06.2026 | 8 min read | Ben Frazer

The conversation around data centers is moving fast—but not always in a clear direction. Spend time at industry events or read the latest headlines, and you’ll hear a common set of themes: compute capacity, advanced cooling, and the rapid rise of AI workloads. These are important, of course. They are driving unprecedented demand, higher rack densities, and new power requirements that are reshaping how facilities are designed.

The scale of that shift is significant: the International Energy Agency has projected that global data center electricity consumption could exceed 1,000 TWh by 2026 in a high-growth scenario. But they also may overlook a deeper and more consequential shift.

There is a significant transformation happening in the server rack. Which is driving and evolving the way data centers connect to, interact with, and increasingly behave like the power grid itself.

And that changes everything.

A Fundamental Shift: From Energy Consumer to Energy System

In previous decades, the relationship between a data center and the grid was straightforward. The grid supplied power. A data center consumed it.

Reliability was addressed internally—through backup generators, uninterruptible power supply (UPS) systems, and layers of redundancy. Sustainability was managed externally, often through renewable energy procurement.

Power, in this model, was a utility service.

That model is rapidly becoming outdated.

Today’s data centers are connecting directly to high-voltage substations, integrating on-site generation, deploying large-scale battery energy storage systems, and managing increasingly complex internal distribution networks. They operate across multiple voltage levels and interacting directly with grid operators.

In practical terms, they are no longer passive consumers. They are becoming active participants in the energy ecosystem—versatile energy players responsible for managing their own power performance.

This shift is not theoretical. It is already reshaping planning, design, and operations across the industry.

Operating Like a Utility Creates a New Set of Responsibilities

When a data center begins to behave like part of the grid, it inherits many of the same challenges utilities have managed for decades.

That includes responsibility for:

  • High-voltage and medium-voltage electrical infrastructure
  • Asset health across transformers, switchgear, and protection systems
  • Compliance with grid codes and operational requirements
  • Power quality and system stability
  • Coordination between generation, storage, and load

At the same time, the expectations placed on data center operators remain uncompromising. Facilities must still deliver continuous uptime, rapid scalability, and global consistency, often on aggressive timelines driven by business demand.

This creates a new reality.

Power is no longer just an input to the data center. It is a core operational system that must be designed, controlled, and optimized with the same rigor as the grid itself.

Why Power Infrastructure Has Become a Strategic Imperative

Historically, power infrastructure was treated as a foundation—critical, but largely invisible unless something went wrong.

That is no longer the case.

Today, the design of power systems is directly linked to a data center’s ability to:

  • Secure grid connections
  • Accelerate project approvals
  • Scale capacity efficiently
  • Meet regulatory and sustainability requirements
  • Maintain operational resilience

This is where Hitachi Energy sees the market evolving—and why solutions are increasingly designed to support continuous operation and uptime while enabling standardized deployment across global footprints. And with high-availability automation approaches delivering up to 99.999% uptime, the bar for performance has risen significantly.

The implication is clear: Power infrastructure is no longer a background capability. It is a strategic differentiator.

The Hidden Layer: Why Automation Is the Real Enabler

Despite the growing complexity of power systems, much of the industry conversation still focuses on physical infrastructure—transformers, switchgear, cooling systems. These are essential components. But they are only part of the story. What determines whether a modern data center operates at peak performance is the layer that connects and coordinates these components: the automation system.

Think of it as the digital backbone of power architecture.

In a grid-like environment, this layer must enable:

  • Real-time monitoring of electrical systems across HV, MV, and LV levels
  • Seamless coordination between substations, storage systems, and internal loads
  • Fast, automated responses to new AI workloads, faults and disturbances
  • Secure communication across operational technology environments

At Hitachi Energy, solutions such as DC-HAAS are designed to address this need, delivering standardized, cyber-secure automation architectures built for availability, scalability, and real-time control. Without this level of integration, even highly redundant infrastructure can fail to perform as intended.

With it, data centers gain the ability to operate a utility-grade power system internally—with the visibility and control required to maintain performance at scale.

Availability Is Expected. Flexibility Is Differentiating

For years, uptime has been the defining metric of data center performance.

Today, it is only the starting point.

The next critical requirement is flexibility.

Modern workloads—particularly AI training and inference environments—introduce far more dynamic power profiles, including high-density compute, large step changes in load, and rapid ramp rates. These behaviors can have a direct impact on grid stability. In the United States alone, EPRI projects data centers could consume 9% to 17% of total electricity by 2030, up from roughly 4% to 5% today. In response, grid operators are introducing more stringent requirements for connection and operation, including:

  • Voltage ride-through capabilities
  • Ramp-rate controls
  • Load smoothing
  • System response during grid events
  • Demonstrated compliance with operational standards

To meet these requirements, data centers are increasingly deploying:

  • Battery energy storage systems (BESS) to smooth load variability
  • Energy hubs that integrate generation, storage, and demand management
  • Advanced power quality solutions to mitigate disturbances
  • Power conversion systems and new distribution architectures

These capabilities allow operators not just to consume energy, but to actively manage how their systems behave within the grid.

And that creates a competitive advantage.

Facilities that can demonstrate flexibility are better positioned to secure grid access, accelerate approvals, and in some cases participate in grid services.

Grid-to-Rack: Redefining Power Efficiency and Design

One of the most important architectural shifts underway is the move toward grid-to-rack power distribution. Traditional designs involve multiple conversion stages, from high-voltage AC down to low-voltage DC at the server level, introducing inefficiencies and complexity.

New approaches, including 800V DC distribution, aim to streamline this process by reducing the number of conversions required.

The result is:

  • Improved energy efficiency
  • Reduced system complexity
  • Higher power density at the rack level
  • Greater control over energy delivery

These innovations are not incremental improvements.

They represent a rethinking of how power flows through the data center—and how that flow can be optimized for performance and scalability.

The Race to Scale: Why Standardization Matters

At the same time, operators are under pressure to deliver new capacity faster than ever before. The challenge is clear: how to scale quickly without introducing unnecessary risk or complexity. The answer increasingly lies in standardization.

Rather than designing each facility from scratch, leading organizations are adopting modular, pre-engineered solutions that can be replicated across regions and adapted to local requirements.

Approaches like DC-HAAS provide:

  • Pre-validated reference designs across HV, MV, and LV systems
  • Standardized architectures aligned with industry standards
  • Reduced engineering and delivery timelines
  • Improved consistency and repeatability

This “design once, deploy many” model allows operators to balance speed with reliability.

And in a market where time-to-power can determine success, that balance is critical.

A Lifecycle View: From Planning to Performance

Another key shift is the move from component-level thinking to lifecycle system management.

  • Data center operators are increasingly looking for integrated solutions that support every phase of the power journey. Hitachi Energy’s approach spans planning, build, operate, and maintain—helping customers bring greater visibility, control, and resilience to increasingly complex power environments: Planning:
    • Grid studies, system design, and configuration optimization
    • Build: Modular grid connections, substations, and automation systems
    • Operate: Real-time monitoring, control, and performance optimization
    • o   Maintain: Asset management, predictive maintenance, and lifecycle services

This integrated approach enables operators to maintain visibility and control across the entire system, improving both reliability and long-term performance.

It also reflects a broader trend: the convergence of infrastructure, digital solutions, and services into a single, unified model.

The Bigger Picture: A New Role for Data Centers in the Energy System

Taken together, these changes point to a broader transformation. Data centers are no longer just digital infrastructure. They are becoming critical components of the energy system itself.

They connect directly to the grid.
They influence how energy is consumed and managed.
They require utility-grade solutions to operate effectively.

And as demand continues to grow, their role will only become more significant.

The Bottom Line: The Future of Data Centers Is Powered by Power

The narrative around data centers will continue to evolve. There will always be new technologies, new workloads, and new innovations to discuss.

But beneath all of it, one truth is becoming increasingly clear:

  • The success of the next generation of data centers will be defined not just by how they compute—but by how they manage power, especially as AI data center demand pushes capacity, flexibility, and resilience requirements to new levels. 
  • Power infrastructure will determine how fast facilities can scale
  • Automation will define how reliably they can operate
  • Flexibility will shape how effectively they integrate with the grid
  • Standardization will enable how efficiently they can be deployed

In short, the future of digital infrastructure is inseparable from the future of energy.

The data center is no longer just a customer of the grid.

It is becoming a critical part of it.

And the operators who recognize that—and build accordingly—will be the ones shaping the next decade of growth.


Ben Frazer

Ben brings more than 20 years’ experience across roles including leading engineering teams, managing operational P&L, and building and scaling organizations. He works closely with global and regional teams on complex, large‑scale energy and digital infrastructure projects driving the energy transition. Ben offers a pragmatic perspective on how technology, planning, and partnership deliver real‑world impact.