Selecciona tu región e idioma

Menú

Panoramic of the border between Spain and France from Jaizkibel, are the towns of Hendaye, Hondarribia, and the French coast of the Atlantic Pyrenees

Biscay Gulf

Customer Story | 2 min read

The Biscay Gulf interconnection project, consists of two HVDC links, connecting France and Spain via a subsea cable across the Biscay Gulf

The Biscay Gulf HVDC interconnection is an HVDC Light® project, enabling power transmission between Spain and France.

The interconnection is made of two parallel links between Gatika, near Bilbao in Spain and Cubnezais, near Bordeaux in France and the system is designed to deliver 2x1,000 MW of electricity at 400 kilovolts (kV) over 400 kilometers (km).

Each of the links consists of two HVDC converter station and both links are constituted of symmetric monopolar systems, at a nominal DC voltage of ± 400 kV.

Each converter station has the feature to operate as a STATCOM and during this operation mode, stations can independently operate within the full capability of reactive power. The system also includes, for all converter stations, the capability to start up a black AC network, up to the full converter capability.

The link will improve safety, stability and quality of the electricity supply between the two countries. It will advance the integration of emission-free electricity and create a more efficient system to generate savings that benefit consumers and the rest of Europe.

Main data

Commissioning year:

2027

Configuration

Symmetrical monopole

Power Transmitted

2,000 megawatts (2 × 1,000 megawatts)

Direct Voltage

±400 kilovolts

Application 

Interconnecting grids