Selecciona tu región e idioma

Menú

Hitachi Energy celebrates the inauguration of Pattern Energy’s SunZia project, now delivering clean, reliable power to millions across the American Southwest

Press Release | New Mexico, United States | 19.06.2026 | 3 min read

  • Hitachi Energy’s HVDC Light® technology is powering Pattern Energy’s SunZia project, easing grid congestion in the Southwest while addressing fast-growing energy demand
  • The system can deliver up to 3,000 megawatts (MW) of clean power from New Mexico to the grid in Arizona, where it can be distributed throughout the region
  • SunZia is the third HVDC Light system commissioned by Hitachi Energy in the last 6 months across the U.S. and Canada, adding a combined 5,450 MW of transmission capacity

Marking a major milestone for transmission infrastructure in the United States, Hitachi Energy, a global leader in electrification, together with Pattern Energy, a leader in clean energy and transmission infrastructure, have announced that the new SunZia Transmission line is now fully operational and delivering power to customers throughout the Southwest.

This high-voltage direct current (HVDC) link transmits 3,000 MW of clean power from the SunZia Wind generation site in New Mexico across roughly 550 miles of overhead lines through remote terrain to the power grid in Arizona. Helping address fast-growing electricity demand in the U.S., the project will supply power to around 3 million people across the Southwest, while supporting rising electricity demand driven by data centers, electrification, and industrial growth.

SunZia Transmission uses Hitachi Energy’s HVDC Light® technology, a state‑of‑the‑art Voltage Source Converter (VSC)-based solution with advanced power electronics to precisely control voltage and power flow. Engineered for long‑distance, high‑efficiency transfer of power with minimal losses, this technology improves grid stability and enables the smooth, reliable integration of energy generated by SunZia Wind.

Hitachi Energy applied its unmatched project execution capabilities, honed through the deployment of some of the world’s biggest and most complex energy infrastructure projects, to successfully deliver SunZia Transmission. This ±525 kilovolt (kV) bipolar HVDC link is the largest VSC-based HVDC installation in the United States and one of the largest worldwide. 

Projects like this show how advanced transmission technology can connect new energy sources from remote areas to the places where it’s needed most. SunZia is an important step toward strengthening the grid and meeting fast-growing energy demand across the U.S., including the rapidly expanding data center market.

Andreas Berthou
Executive Vice President HVDC
Hitachi Energy

For SunZia, HVDC is not just a technology choice, it’s the project’s key differentiator. Hitachi Energy’s HVDC technology is what allows large amounts of power generated in New Mexico to move efficiently across long distance. SunZia is proof of what HVDC can do: connect regions, improve efficiencies of the market and enhance reliability.

Hunter Armistead
Chief Executive Officer
Pattern Energy

SunZia will also help balance energy supply and demand, addressing the ‘duck curve’1 that occurs when solar generation drops in the evening and demand for electricity remains high. The VSC based HVDC system can rapidly adjust power flow, allowing the grid to respond quickly to changing conditions while delivering more wind energy precisely when it’s needed, reducing reliance on fossil fuel plants during peak periods. Paired with ultra‑fast AC choppers, the system is designed to protect grid stability, ensure reliable, consistent energy delivery even during weather disruptions or other unexpected events.

Advancing progress toward Arizona’s energy independence, SunZia is expected to avoid approximately 9 million metric tons of CO₂ in its first year of full operation. This is the equivalent of removing three million gasoline-powered cars from the road for an entire year2.

SunZia is the third major HVDC Light project commissioned by Hitachi Energy in the United States within the last 6 months, significantly strengthening the grid at a time when demand growth is outpacing supply.

About Hitachi Energy

Hitachi Energy is a global leader in electrification, powering the electricity era to meet the energy demands of today, and the next 25 years. As the energy arm of Hitachi Group, over three billion people depend on our pioneering, mission-critical technologies to power their daily lives. With over a century of innovation, we are addressing the most urgent energy challenge of our time: driving the evolution of the world’s energy system to ensure abundant, secure, affordable, and sustainable power for today’s generation and the next. With an unparalleled installed base in over 140 countries, we are the grid ecosystem partner across the utility, industry, data center, and transportation sectors. Headquartered in Switzerland, we employ over 56,000 people in 60 countries and generate revenues of around $20 billion USD.

https://www.hitachienergy.com
https://www.linkedin.com/company/hitachienergy
https://x.com/HitachiEnergy

About Hitachi, Ltd.

Through its Social Innovation Business (SIB) that brings together IT, OT (Operational Technology) and products, Hitachi aims to be a global leader in continuously transforming social infrastructure through digital, contributing to a harmonized society where the environment, wellbeing, and economic growth are in balance. Hitachi operates worldwide across four sectors – Digital Systems & Services, Energy, Mobility, and Connective Industries – as well as a Strategic SIB Business Unit focused on new growth areas. With Lumada at its core, Hitachi creates value by combining data, technology and domain knowledge to solve customer and social challenges. Revenues for FY2025 (ended March 31, 2026) totaled 10,586.7 billion yen, with 606 consolidated subsidiaries and approximately 290,000 employees worldwide. Visit us at https://www.hitachi.com.

Contacts

Photo of
Media Relations

Hitachi Energy

Get to know more