Choose your region and language

Go

Menu

Team of main engineers control of industry process using SCADA system, AI and digital technology. Operators control machine operation processes uses screens. Industry 4.0

Keeping the power grid secure

Summary 


As if natural disasters aren’t reason enough to be concerned, physical attacks on substations have many in the industry rethinking substation resiliency. About once every four days, part of the nation’s power grid is struck by a cyber or physical attack. Resiliency and reliability of the power grid are critical to our everyday lives, economies, and critical infrastructures such as hospitals, first responders, government facilities, and so on, so making sure it is protected and secure is of utmost importance. Join Dustin Prescott, former Hitachi Energy employee, and grid integration subject-matter expert, as he discusses the steps to keeping the power grid secure and safe from natural disasters and physical attacks.

Featured links

Connect with Dustin on LinkedIn

Get to know more