Choose your region and language

Go

Menu

Connecting one of the world’s largest solar-and-battery projects to the Philippine power grid

Customer Story | 4 min read

The Philippines is trying to rely less on imported fuel and more on the power it generates at home. Two government programs are pushing that shift: the National Renewable Energy Program and the Green Energy Option Program (GEOP), which lets large electricity users buy power directly from renewable suppliers instead of the regular grid mix. Together, these programs support a national target of 35% renewable energy by 2030 and 50% by 2040.

That ambition is now taking shape in one of the world’s most significant solar-and-battery storage developments. Designed to combine 3,500 MWp of solar generation with a 4,500 MWh battery energy storage system, the project is set to become one of the world’s largest hybrid solar facilities.​

The Challenge

Supporting the country’s clean energy goals with renewables

Developing one of the world's largest integrated solar-and-battery facilities required more than installing generation capacity. It required ensuring that vast amounts of renewable energy could be transferred safely, efficiently, and reliably into the national grid.

Integrating gigawatt-scale renewable generation presents significant challenges for grid operators, including maintaining system stability, ensuring reliable power transmission, and supporting the long-term resilience of the electricity network.  These challenges are amplified in a project of this scale, spanning across 3,500 hectares, covering six municipalities in the Nueva Ecija and Bulacan regions, and connecting them to the Luzon grid through a 13-km 500-kV transmission network.

To realize the full value of the project, a robust electrical infrastructure was required, with transformers playing a critical role in stepping up and stabilizing the power needed to enable secure grid connection and dependable delivery to homes, businesses, and communities across the Philippines.

The Solution

Transformers enabling efficient large-scale solar power integration

To support the project's grid connection requirements, Hitachi Energy supplied 10 x 260 MVA power transformers and 14 earthing transformers. Together, these transformers form a critical link between renewable generation and the national grid.

  • The power transformers serve to step up the electricity generated by the solar facility to 500 kV, enabling efficient transmission from the site to the Luzon grid while minimizing energy losses.
  • The earthing transformers provide essential grounding and protection functions, helping operators detect faults and maintain the safety and resilience of the network.

The timely delivery of this critical equipment helped keep the project timeline on schedule. By meeting key project milestones, the on-time delivery of the transformers supported seamless grid integration, helped avoid delays, and enabled the project's successful progression from construction to operation.

Adani’s solar power plant in Kamuthi

The Impact

Turning ambition into reliable power

In July 2026, Phase 1 of the project was successfully energized, bringing 1,373 MW of solar capacity and 825 MW (3,300 MWh) of battery storage online. That made it one of the largest operational integrated solar-and-battery facility on a single site in the world.

Upon full completion in 2027, it is set to deliver enough renewable energy to meet roughly 12% of the Philippines' electricity demand, power approximately 2.4 million homes, and avoid an estimated 4.3 million tons of carbon emissions each year.

For the Philippines, the project represents more than new renewable capacity. It supports energy security, reduces reliance on imported fuel, and helps advance the country’s transition toward a cleaner, more resilient power system. For Hitachi Energy, it demonstrates how transformer technology enables renewable energy to move safely, efficiently, and reliably from landmark renewable projects into the grid.

At this scale, the energy transition is not an abstract ambition. It is built through infrastructure: the power equipment that connects generation to the grid, keeps power flowing, and helps millions of people benefit from cleaner electricity.

Hitachi Energy contributed to one of the world’s most significant solar energy developments. In the Philippines, we have supplied 10 custom-built 260 MVA, 230 kV power transformers and 14 units of zigzag dry-type transformers. This equipment provides the critical ground and reliability required for safe and stable grid operations and is manufactured using 100% fossil-free electricity. These transformers reflect our core commitment to innovation, sustainability, and delivering the energy systems of tomorrow.

Rodolfo Indorte
Country Managing Director, Philippines
Hitachi Energy

Powering solar and storage at scale

Reliable transformer solutions for solar PV and battery energy storage, from power conversion to grid integration.