Escolha a sua região e idioma

Ir

Menu

The opportunity:

We seek a Control Design Engineer for power quality solutions mainly synchronous condenser with medium to high complexity. This function will include complete assignments on medium to large projects requiring engineering that is cost-effective and in accordance with contract specifications, quality standards and safety requirements. Based on technical specification from end customers and inputs from Operating Unit Engineering teams, it is required to prepare system Communication Block Diagram, Network topology, IP list, I/O signal list and Internal validation of RTU, PLCC based system. Furthermore, this function includes work on standard technical specifications for major equipment, providing input to R&D activities for plant base solutions. Cost awareness and carrying out comparisons between different solutions, bill of materials, RFQs, vetting of vendor offers, engineering hours estimation, technical risk assessment and opportunity evaluation is also required.

How you’ll make an impact:

  • Design of Communication Block Diagram along with network topology based on specifications. Design and verify the HMI application for various PQ Control and Protection System.

  • Configuration of SCADA Gateways, Engineering workstation, Network switches, GPS, KVM, GOOSE. Configuration of SCL, CID, ICD files.

  • Creation of I/O signal list, SCADA Signal list. Control logic design and internal validation. Undertake PSCAD and RTDS simulation studies individually or as part of a team to verify control dynamic performance of FACTS solution.

  • Support tenders, delivery projects, and R&D activities during control system dynamic performance studies Lead, supervise and coordinate engineering project teams and towards other departments related to scope, schedule & progress, approvals, budget, targets, resource load & cost-to-complete.

  • Ensure Engineering processes and base solutions are applied. Conduct engineering project reviews and report progress and cost-to-complete engineering- and project manager.

  • Establish contacts with suppliers for technical support to improve material quality and/or to optimize on costs. Prepare base design and detailed designs and focus on continuous improvements both technically and functionally.

  • Track and handle technical issues and follow up. Handle clarification where more than one domain/function/party is concerned plus topics that cannot be allocated to an engineering domain. Initiate mitigation of possible responsibility gaps in the project team.

  • Collect and consolidate project risks and opportunities from engineering team, technical, but as well related to engineering work, information/data availability and assumptions taken. Define, coordinate & take proactive actions to mitigate risks.

  • Responsible for ensuring compliance with applicable external and internal regulations, procedures, and guidelines.

  • Living Hitachi Energy’s core values safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background:

  • Minimum bachelor’s degree (B.E/B.Tech) in electrical engineering, with minimum 6-7 years of work experience. Prior experience in SAS most preferred.

  • Cyber Security exposure for SAS and PQS systems will be added advantage. Knowledge on communication protocols like Mod Bus, DNP3, IEC 101/104, TCP/IP, PRP, HSR, etc.

  • Knowledge on RTU til 500 and Multiprog PLC (Preferred) Strong knowledge on IEC 61850 (MMS and GOOSE). Configuration of IEC61850 in different vendor relays (SEL, HITACHI, GE) System Integration of different product IED, meters and other substation devices into RTU/Gateway .

  • Basic power system knowledge to understand the Sync Con operation. Basic Protection knowledge on IED’s Configuration of GPS, Ethernet switches and network components configurations.

  • Hands on experience on System network preparation/topology for validation and testing along with test procedure.

  • Exposure in commissioning support for HMI / SCADA Knowledge of T&D equipment, such as AC / DC switchgear circuit breakers, disconnectors, earthing switches, instrument transformers, power transformers, cables.

  • HV & MV substation engineering understanding and experience preferred. Technical risk and opportunity assessment and validation Take ownership for the project KPIs such as OTD, COPQ etc. Estimation of engineering effort for each project for costing at tender stage Innovativ ideas to reduce engineering effort.

  • Proficiency in both spoken & written English language is required.

Localização Chennai, Tamil Nadu, India
Tipo de emprego Full time
Experiência Experienced
Função do trabalho Engineering & Science
Contrato Regular
Data de publicação 2026-05-13
Número de referência R0112157

Sobre a Hitachi Energy

A Hitachi Energy é uma líder global em tecnologia que está promovendo um futuro de energia sustentável para todos. Atendemos clientes nos setores de serviços públicos, indústria e infraestrutura com soluções e serviços inovadores em toda a cadeia de valor. Juntamente com clientes e parceiros, somos pioneiros em tecnologias e possibilitamos a transformação digital necessária para acelerar a transição energética para um futuro neutro em carbono. 

Empregamos mais de 45.000 pessoas em 90 países que todos os dias trabalham com propósito e usam suas diferentes origens para desafiar o status quo. Convidamos você a se inscrever hoje e fazer parte de uma equipe global que valoriza uma verdade simples: Diversidade + Colaboração = Grande Inovação.