Selecciona tu región e idioma

Menú

The opportunity:

HVDC (High Voltage Direct Current) is a product group in Hitachi Energy, which develops, manufactures and sells DC transmission systems on a global market. HVDC technology is used to transmit electricity over long distances and for power transmission via submarine cables. It is also used to connect power systems. We are now hiring a Completion Manager to HVDC Sweden, a business line within Hitachi Energy. As Completions Manager you have a key role in the project by being responsible to define and implement the Project Completion Strategy. You will have the opportunity to work both operational and strategic, as well as interacting with different internal and external stakeholders within the business.

How you’ll make an impact:

  • Define the Project Completion System/s (PCS) and interfaces in the Projects, identify engineering inputs, tools and dataflow to feed engineering data into the PCS.

  • Setup the project PCS structure.

  • Receive, validate and process source data, engineering lists and technical drawings to populate the PCS in line with the project requirements and the Project Completion Strategy.

  • Populate the PCS for procurement activities in conjunction with the Master Test Plan.

  • Implement the Completions scope of work for ITR check sheets, create project specific ITR templates as required from Construction & Commissioning approved documentation.

  • Manage the PCS regarding user access, admin, guidance and training.

  • Support the Project Completion Manager creating the Preservation activities in the PCS, support the projects in punch list data imports, updates and maintenance based on the project needs, support creating reports and monitoring the project Completions KPIs.

  • Receive, validate and process change control notices relating to data (engineering lists, drawings, users) held or processed by the PCS and update the project's scope accordingly.

  • Responsible to ensure compliance with applicable external and internal regulations, procedures, and guidelines.

  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background:

  • Technical / Engineering / Quality management education.

  • Minimum 2+ years professional experience, and/or completion of at least one major project up to handover to the Customer, in a role related to the function within an EPC in Power, Energy or Oil & Gas project(s).

  • Experienced working with a Project Completions Systems (PCS) preferably with PIMS or other PCS such as ProCoSys, WinPCS, etc.

  • Proficient oral and written communication skills including technical documentation and reporting.

  • Sensitive to Customer and project team needs and can develop a sustainable relationship to all involved stakeholders through clear communication, influencing and coordination.

  • English fluency (written + spoken),

Ubicación Chennai, Tamil Nadu, India
Tipo de empleo Full time
Experiencia Experienced
Función laboral Quality Management
Contrato Regular
Fecha de publicación 2026-04-30
Número de referencia R0122661

Sobre Hitachi Energy

Hitachi Energy es un líder tecnológico mundial que está promoviendo un futuro energético sostenible para todos. Prestamos servicios a clientes de los sectores de servicios públicos, industria e infraestructuras con soluciones y servicios innovadores en toda la cadena de valor. Junto con clientes y socios, somos pioneros en tecnologías y facilitamos la transformación digital necesaria para acelerar la transición energética hacia un futuro neutro en carbono.

Empleamos a unas 45.000 personas en 90 países que cada día trabajan con un propósito y utilizan sus diferentes orígenes para desafiar el status quo. Te invitamos a presentar tu candidatura hoy mismo y a formar parte de un equipo global que aprecia una simple verdad: Diversidad + Colaboración = Gran Innovación.