Choose your region and language

Go

Menu

Steam rises from a new ammonia production unit currently under testing at a fertilizer plant in Russia. Photographer: Andrey Rudakov/Bloomberg

Electrification for a low-carbon future: Turning round-the-clock green power into Green Ammonia in India

Customer Story | 4 min read

In Kakinada, on India’s eastern coast, an existing ammonia and urea complex is being converted into a large-scale renewable ammonia production facility, becoming one of the world's largest green ammonia and green hydrogen production facilities. 

The project will use renewable electricity to produce green hydrogen through electrolysis, before combining that hydrogen with nitrogen to create green ammonia. Once fully operational, the facility is expected to produce one million tonnes of renewable ammonia annually and avoid approximately two million tonnes of CO₂ emissions each year. 

Green ammonia is becoming increasingly important because it connects renewable electricity and hydrogen with industrial applications that can be difficult to decarbonize through direct electrification alone. Green hydrogen provides the essential building block, while converting it into ammonia creates a versatile product that can serve as a lower-carbon feedstock for industries such as fertilizers and chemicals, as well as an energy carrier with potential applications in shipping and power generation.

The Challenge

Delivering renewable power in a form electrolysers can use

Producing green ammonia begins with green hydrogen. At Kakinada, pressurized alkaline electrolysers will use renewable electricity to split water into hydrogen and oxygen. The hydrogen will subsequently be used in the ammonia-production process, creating an alternative to conventional ammonia production based on fossil fuels. The project is being developed through two electrolyser phases of approximately 640 MW each. 

However, supplying renewable electricity to the site is only part of the challenge. Electrolysers operate on controlled direct current, while the plant’s electrical network supplies alternating current. Before that electricity can support hydrogen production, it must therefore be transformed to the required voltage and then converted from AC to DC. At this interface between renewable power and the electrolysis process, rectifier transformers become a critical part of the electrical system.

The Solution

Transformer technology supporting large-scale electrolysis

Working in collaboration with Hubei Green Power, Hitachi Energy is supplying 64 rectifier transformers, each rated at 15.58 MVA and 33 kV, for integration into the rectifier power-supply system. Green Power will integrate the transformers into the complete power-conversion equipment before the system is delivered to the Kakinada project. 

The transformers adapt the incoming AC electricity to the operating requirements of the rectifier system. The rectifiers then convert that electricity into the controlled DC power required by the electrolysers. Together, these technologies enable renewable electricity to reach the hydrogen-production process in a usable and controlled form.

The Impact

Enabling the connection between clean power and industrial decarbonization

The Kakinada project demonstrates how renewable electricity can be converted into green molecules for industrial use. The combination of renewable generation, energy storage, large-scale electrolysis and ammonia production creates a pathway from clean power to applications where direct electrification may not always be practical.

Within this wider ecosystem, the rectifier transformers provide an essential connection between the electrical network and the electrolysers. By helping deliver power at the voltage and in the form required for electrolysis, the Hitachi Energy solution supports the production of green hydrogen and, ultimately, renewable ammonia at scale.

The project also illustrates the importance of collaboration across the value chain. By combining Hitachi Energy’s transformer expertise with Green Power’s power-conversion system capabilities and the wider project partners’ electrolysis and ammonia-production technologies, the Kakinada facility can help advance lower-carbon industrial production and the development of an international renewable-ammonia supply chain.

Hydrogen renewable energy production - hydrogen gas for clean electricity solar and windturbine facility.

Explore transformer solutions for hydrogen applications

Discover transformer solutions enabling renewable electricity for hydrogen production.