Hitachi Energy and Fingrid partner to enhance Finnish grid development with large power transformers
Press Release | Europe | 26.06.2026 | 1 min read
Hitachi Energy, a global leader in electrification, has entered into an agreement with Fingrid, Finland's transmission system operator, to deliver seven large power transformers, each with a capacity of 400 MVA and operating at 400 kV. This contract is a pivotal part of reinforcing the Finnish electricity grid and includes the option to supply two additional transformers.