Choose your region and language

Go

Menu

Special requirements for Power Transformers connected to the grid


The TXpert ecosystem includes the TXpert HUB (Coretec) and the Coresense, a TXpert enabled sensor for DGA monitoring.

Both drive the need to get real-time information from remote areas and this real-time monitoring of assets to help users being informed about their future decisions.  

We expect users to enhance the maintenance of their transformers by using this technology.

Enabling digital technologies in transformers allows customers to get vital information and run advanced analytics that support a more efficient and reliable network.

If a transformer is located in a remote area, to monitor the transformer, Coretec and Coresense (DGA) are good devices to utilize. 

The TXpert ecosystem with the Coretec HUB provides the right features to evaluate transformer’s life time and efficiency digitally by using mathematical methods.

Sessions

Presenters

Hashim Malik

Digital Lead for Middle East & Africa
Hitachi Energy

MBA International Commercial from Stockholm, Sweden.

Over the past 11 years, he held several positions in Hitachi Energy covering HVDC Transformers, LMPT Transformers, Service Transformers and worked in several countries.

Currently based in Dubai as Digital Lead for Hub APMEA (Asia Pacific Middle East and Africa) originally, his home base is Ludvika, Sweden.

Sezgin Perdahci

Product Marketing Manager for Power Transformers
Hitachi ABB Power Grids

MSc of Electrical Engineer with more than 22 years of experience in Power Transformer business.

First 10 years, I had been Sales Engr. in Power Transformers – Kartal Plant

Following 5 years, I had been Area Manager for Middle East of Kartal Plant.

Between 2014 and the end of 2019, I had been Sales & Marketing and Order Handling Manager of Kartal Plant.

Currently, I am based in Kartal Plant as Product Marketing Manager for Power Transformers.

Available on demand

Special requirements for Power Transformers connected to the grid.