Choose your region and language

Go

Menu

The Next Generation of Energy Management Systems: Gridsof the FutureRequire Coordinated Control

Blog Post | 11.05.2026 | 7 min read | Jean-Marc Moulin

The energy landscape is undergoing one of the most profound transformations in its history. Accelerated renewable integration, declining system inertia, electrification of demand, and increasing volatility are fundamentally changing how power systems behave—and how they must be operated. At the center of this transformation is the Energy Management System (EMS).

EMS platforms are no longer passive tools that monitor and alarm. They are becoming the digital backbone of grid operations. They actively coordinate assets, data, and decisions across the entire value chain.

Looking ahead, the future of EMS is defined by two critical dimensions: 1) Coordinated control across transmission and distribution, and 2) the ability to react faster than ever before.

Dimension One: Coordinated Control Across Transmission and Distribution

Historically, power transmission and distribution have been managed as largely separate operational domains. That separation is no longer sustainable as the lines between the two continue to blur.

As the generation mix evolves, the traditional distinction between transmission and distribution is becoming increasingly difficult to maintain. The industry often describes this transition as a shift toward a “50/50 split” between bulk and distributed resources, but this simplification no longer reflects reality. 

Much of the growth in renewables, particularly wind and increasingly solar PV, is occurring at grid scale, meaning these assets operate like bulk generation regardless of technology. However, their classification depends on where they are connected. Some are integrated into transmission networks through EMS and TSO environments, while others are connected at the sub-transmission or distribution level through ADMS and DSO systems. As a result, connection point, rather than size or system impact, determines how these resources are categorized, introducing significant ambiguity.

Even rough estimates, such as bulk generation representing around 70–75% of capacity, mask a more complex reality. A meaningful share of these bulk-like resources is now connected within distribution networks, blurring operational boundaries and making it difficult to assign clear percentages between transmission and distribution domains. 

The issue is no longer just about shifting proportions, but about the breakdown of the categories themselves. Grid-scale renewables and distributed energy resources are creating a more interconnected system in which traditional distinctions no longer align with how assets behave or how the grid must be managed.

 

This is why the future EMS must enable close coordination across transmission and distribution. This coordination does not require unified ownership, but it does depend on closed-loop data exchange and shared situational awareness. Transmission system operators need real-time visibility into downstream activity, including rooftop solar, batteries, EV charging, flexible demand, and sub-transmission networks. In parallel, distribution operators need awareness of upstream constraints, voltage conditions, and system-wide stability risks.

Modern EMS platforms are increasingly evolving into the central coordination layer, integrating data from across the enterprise. Asset Performance Management and Work Management systems, Market Management Systems, advanced forecasting tools, Wide Area Monitoring Systems, and even intelligent field devices all contribute to a richer operational picture. Bringing these sources together allows operators to move from reactive management toward proactive, system-wide coordination.

The experience of forward-looking utilities illustrates this shift. In Slovenia, for example, the transmission system operator ELES is deploying its own applications directly on top of its Network Manager EMS platform, demonstrating how open and interoperable architectures enable utilities to innovate without being constrained by rigid systems. Similarly, a North American ISO operates one of the most tightly integrated EMS and Market Management environments, using the EMS itself to test congestion scenarios for market clearing. This reflects a broader move toward tightly coupled operational and market coordination at scale.

Dimension Two: The Need to React Faster

As coordination needs become broader, the second defining requirement of next-generation EMS is speed.

Grid reaction times are shrinking from minutes, to seconds, and increasingly toward milliseconds. In a system dominated by inverter-based resources, reduced inertia, and fast-changing power electronics, there are scenarios where human operators simply cannot react quickly enough to maintain stability. Oscillations, voltage instability, and frequency events may require action before an operator can fully assess the situation.

This reality is driving a fundamental shift in how EMS platforms support decision-making. Artificial intelligence and machine learning will be increasingly used to guide what should happen next and why, not just report what has already occurred. Advanced forecasting of load, renewable generation, constraints, and even system inertia allows operators to see risk developing hours or minutes in advance.

At the same time, automation is becoming central to grid operations. Instead of executing manual control actions, operators are evolving into supervisors of an automated world. Machines analyze vast amounts of data, trigger pre-approved control actions, and present operators with clear explanations of the “why,” not just the “what.” This human‑machine partnership is essential for managing complexity at modern grid speeds.

Importantly, this evolution is not instantaneous. The industry is on a journey. It is moving from operator-driven control, to operator-assisted automation, and eventually toward higher levels of autonomy in defined situations. Most utilities see the future landing with deeper levels of automation wherein systems act independently under certain conditions, while keeping human operators firmly in command.

What Happens If Utilities Don’t Evolve?

The consequences of standing still are significant. Reduced inertia, increasing system strength challenges, and volatile demand mean that traditional EMS approaches struggle to cope not only with today’s dynamics, but even more with tomorrow’s. As discussed in industry forums and reflected in recent major outages, grid disturbances are rarely caused by a single factor. They are the result of multiple stresses acting simultaneously across the system.

Without faster analytics, intelligence, and coordinated automation, operators may be forced into making crude interventions, such as load shedding at the transmission level. In the long run, failing to modernize EMS capabilities risks reliability, market efficiency, and public trust.

Differentiation That Matters

Not all EMS platforms are equally equipped to meet these challenges. What differentiates leading solutions is the depth and breadth of their portfolios. When an EMS is part of a broader ecosystem, for example spanning grid automation, asset management software, markets systems, digital analytics solution, and hardware, it can extract far more value from data that already exists across the enterprise.

Equally important is field-proven performance. Next-generation EMS platforms must be reliable, secure, and scalable, operating some of the largest power systems on earth. Innovation matters. But only when it is grounded in systems that work at scale, under real-world conditions, every day.

Finally, new technologies such as AI and machine learning are no longer experimental add-ons. They are embedded capabilities, used today for forecasting, alarm intelligence, security analysis, and operator decision support, paving the way for faster, safer, and more resilient grids.

The Trend Behind It All

The single biggest force driving EMS evolution is the energy transition itself. Rapid growth in renewables, declining inertia, electrification of transport and industry, the rise of batteries and data centers are some of the notable changes coming from every angle at once. The grid is becoming more complex, more dynamic, and more critical than ever.

In response, the EMS is transforming from a control-room tool into a strategic platform: orchestrating across transmission and distribution, reacting at machine speed, and empowering human operators to manage complexity with confidence.

The next frontier of grid operations will belong to those who can see across boundaries and act before instability becomes inevitable.

Frequently Asked Questions

A next-generation EMS is an advanced platform that goes beyond monitoring to actively coordinate grid operations across transmission and distribution, using real-time data, automation, and AI-driven insights to improve reliability and efficiency.

As more renewable and distributed energy resources connect across the grid, transmission and distribution systems must operate as an integrated whole. Coordinated control ensures better visibility, faster response to instability, and more efficient use of grid assets.

Modern EMS platforms leverage advanced forecasting, machine learning, and automation to detect risks earlier and initiate faster responses. This enables operators to manage increasingly dynamic grids where events unfold in seconds or even milliseconds.


Jean-Marc Moulin

Jean-Marc Moulin has more than 35 years of experience in the Electrical utility domain, ranging from Generation to Transmission and Distribution, encompassing solutions development, deployment, and next-generation definition. His portfolio includes GMS, EMS, WAMS, ADMS, Utility DERMS, and Markets (MMS). He is also a frequent keynote speaker at international conferences such as CIGRE, EPEx, EPCC, Next Gen SCADA, and DTECH.