Scegli la tua regione e lingua

Vai

Menu

Business Information

Hitachi Energy is currently looking for a GIS Secondary Engineer for the High Voltage Business to join their team in Savli Gujarat, India. This team seeks a skilled and motivated individual.

Hitachi Energy is a leader in high-voltage technology, offering a wide range of high-voltage products up to 1,200-kilovolt (kV) helping enhance the safety, reliability and efficiency of power networks while minimizing environmental impact. Our technology leadership continues to facilitate innovations in power transmission, enabling smart grids and enhancing eco-efficiency.

Hitachi Energy’s EconiQ™ high-voltage portfolio eliminates SF6 with reliable and scalable solutions for the lowest carbon footprint. The EconiQ line has achieved two world’s first – the replacement of SF6 in existing high-voltage equipment called EconiQ Retrofill and the breakthrough SF6-free 420 kV circuit-breaker. Hitachi Energy has placed sustainability at the heart of its Purpose and is advancing a sustainable energy future for all. 

The ideal candidate must enjoy working in a dynamic, fast-paced business environment. He or she must be flexible in accommodating business requirements and experience in working with diverse groups and cultures. The ability to multitask & deliver within timelines is essential. The candidate will have excellent communications skills.

Mission Statement

You will be a part of the GIS LCC Secondary team and support the execution of LCC engineering. Your work involves mainly creating electrical circuit diagrams and supporting documents. We use the E3 tool for generating the schematics. You will be an individual contributor who would deliver the tasks as per the given inputs and when required need to work in coordination with other colleagues and should exhibit good collaborative skills to complete the task. In the absence of your Lead or in some cases, you will be required to interact with our counterparts to get/clarify queries. You may also interact with other departments like Primary, Project Management, and Production.

Your Responsibilities
  • Preparation of Local Control Cubical schematics for High Voltage Gas Insulated Switchgear (66 kV and above).

  • Preparation of GIS CB / Disconnector / Earthing switch / Fast Acting Earthing switches / CT & VT schematics.

  • Preparation of Junction Box for CT, VT, and Density monitors, AC / DC Load calculation.

  • Preparation of Interlocking table and schematics for various Busbar configurations.

  • Addressing the technical queries raised by the customer during the execution of a project, if required.

  • Interaction with various cross-function teams like Primary, Project Management, and Production, when required.

  • Self-reviewing the documents before submitting them to Lead Engineer . Generating Preliminary BOM by understanding the importance and consequences of releasing it.

  • Preparation of Mimic boards in line with SLD and Layout drawings.

  • Understanding and preparation of Communication Architecture diagrams.

  • Preparation of protection schematics (Trafo, Line, Busbar) when we’ve integrated protection in LCC . Selection of Bay Control Unit and other protection IEDs (Basic level).

  • Preparation of complete Digital LCC drawings as part of Digital Substation (with NCITs, MU’s, SAM600 modules, etc...).

  • Preparation of Gas Density monitoring panels using MSM (Modular Switchgear Monitoring).

  • Adhering to applicable codes, practices, QA/QC policies, performance standards, and specifications.

  • Living Hitachi Energy’s core values safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your Background
  • Bachelor’s degree in B.E / Diploma in Electrical Engineering.

  • Must have 2 -6 years of experience.

  • Excellent knowledge of CAD tools (Good experience in e3, not mandatory).

  • Very Good knowledge of Protection & Control Systems for T & D / Gen.

  • Familiarity with codes and applicable standards like IEC, IEEE, ANSI, etc...

  • Basic knowledge of GIS  Ability to work with multiple discipline projects.

  • Ability to work in a team and maintain professionalism. Good communication and interpersonal skills.

  • Proficiency in both spoken & written English language is required.

Sede Savli, Gujarat, India
Tipo di lavoro Full time
Esperienza Experienced
Funzione lavorativa Engineering & Science
Contratto Regular
Data di pubblicazione 2025-05-22
Numero di riferimento R0091993

Hitachi Energy

Hitachi Energy è un leader tecnologico globale nell'elettrificazione, che promuove un futuro energetico sostenibile grazie a tecnologie innovative per le reti elettriche, incentrate sul digitale. Oltre tre miliardi di persone dipendono dalle nostre tecnologie per dare energia alla propria vita quotidiana.

Con oltre un secolo di esperienza pionieristica nelle tecnologie mission-critical di alta tensione, trasformatori, automazione ed elettronica di potenza, stiamo affrontando la sfida energetica più urgente del nostro tempo: bilanciare la crescente domanda di elettricità con la decarbonizzazione del sistema energetico.

Con sede in Svizzera e oltre 50.000 persone in 60 paesi, Hitachi Energy genera fatturato per circa 16 miliardi di dollari. Candidati oggi stesso!