Scegli la tua regione e lingua

Vai

Menu

Features Zurich, Switzerland 27-01-2016

3 min read

ABB to strengthen power network at world’s busiest international airport

Upgrade of control system to manage growing power network at Dubai International Airport (DXB)

Zurich, Switzerland, January 27, 2016 - ABB, the leading power and automation technology group, will upgrade its SCADA (supervisory control and data acquisition) system for the power network at Dubai International (DXB), the world's busiest international airport. The upgraded system includes replacement of the central computers and deployment of the latest version of ABB's Network Manager software. This will connect to the existing field devices (remote terminal units, bay control units and main distribution boards) and increase the operational reliability and efficiency of the power network to support a large-scale airport expansion plan.

ABB delivered the first SCADA system to Dubai International in 2004 and the monitored network has grown five-fold since then. In addition to augmenting capacity and offering, advanced features include highly efficient real-time alarm and event handling.

ABB's SCADA solution provides a common power distribution automation system and today handles data signals from approximately 100,000 sources distributed over the entire power network at any given time.

As part of the current system, field-based sensors continuously monitor detailed data related to the power network in real time, and provide the operator with analytics to support decision making processes and optimize operations.

"This upgrade will provide advanced automation of the power distribution network and enable reliable and efficient power supplies to the world's busiest international airport, optimizing the use of resources and minimizing disruption to passengers" said Claudio Facchin, President of ABB's Power Grids division. "Grid automation and leveraging our software portfolio to deliver enhanced customer value are key elements of our Next Level strategy supporting our Internet of Things, Services and People approach."

Dubai International is the world's busiest airport for international passenger traffic, with flights to more than 260 destinations. It is also the world's third busiest hub in terms of international air freight. In 2014, it handled more than 70 million passengers and 2.4 million tons of cargo.

A SCADA system enables remote monitoring and control of complex systems. It can be combined with a data acquisition system to acquire information about the status of the remote equipment. These computer-based systems help monitor and control industrial, infrastructure and facility based processes and are extensively used in applications like electrical power transmission and distribution.

About ABB

ABB (www.abb.com) is a leader in power and automation technologies that enable utility, industry, and transport and infrastructure customers to improve their performance while lowering environmental impact. The ABB Group of companies operates in roughly 100 countries and employs about 140,000 people.