Scegli la tua regione e lingua

Vai

Menu

Press Release Zurich, Switzerland 01-11-2021

3 min read

Hitachi Energy contribuisce agli obiettivi di sostenibilità della Scozia con la tecnologia rivoluzionaria EconiQ

View from the Beach of Culzean Castle on the Ayrshire Coast Near Glasgow in Scotland
SP Energy Networks sta contribuendo a raggiungere gli obiettivi di decarbonizzazione evitando l'aggiunta di oltre 3.000 chilogrammi di esafluoruro di zolfo alla rete elettrica di trasmissione

Hitachi Energy will supply SP Energy Networks with pioneering EconiQTM gas-insulated lines (GIL) to support the country’s sustainable energy targets.

Scotland has ambitious goals to decarbonize its energy system and reduce greenhouse gas emissions to net zero by 2045. In its journey towards carbon-neutrality, SP Energy Networks is upgrading the aging energy infrastructure and bringing in advanced technologies to better manage energy flow in the grid.

One such project is the Windyhill 275-kilovolt (kV) substation located northwest of Glasgow. Built in the1960s, the air-insulated substation plays a significant role in the SP Energy Networks transmission network and is now being modernized as part of its RIIO-T21 business plan. It is part of the critical infrastructure node for emergency network recovery.

Hitachi Energy will deliver 1,500 meters of eco-efficient EconiQTM GIL which contains no sulfur hexafluoride (SF6), instead making use of an alternative insulation gas mixture which essentially eliminates the CO2 equivalent emissions throughout the total lifecycle. This avoids the addition of over 3,000 kg of SF6, the equivalent of removing CO2 emissions from around 7,5002 passenger vehicles from the road in a year. The Windyhill substation refurbishment is expected to be completed in 2025.

"We are honored to be SP Energy Networks’ partner of choice in the acceleration of Scotland’s energy transition," said Markus Heimbach, Managing Director, High Voltage Products at Hitachi Energy. “Following more than two decades of intensive R&D, we have been deploying SF6-free high-voltage technologies and helping our customers to reduce their carbon footprint.”

“We’re continuously evolving our operations and looking for ways to make our network more environmentally sustainable. The introduction of this greener technology developed by Hitachi Energy is a major step forward in our push towards achieving Net Zero emissions in the future”, said Pearse Murray, SP Transmission Director at SP Energy Networks. “The eyes of the world are on Glasgow just now with the COP26 climate change conference taking place in the city. Introducing this new technology will have a legacy long beyond COP26 and it cements our position leading the way towards sustainable substations. We’re proud of our innovative approach to delivering a greener future for our customers.”

In addition to the EconiQ TM solution, Hitachi Energy will also deliver 15 bays of its highly reliable and flexible 300 kV gas-insulated switchgear (GIS). A technology pioneered by Hitachi Energy which can be installed in confined spaces and can operate in extreme environmental conditions.

Recently, Hitachi Energy announced the acceleration of its development of eco-efficient solutions and outlined its extensive EconiQ roadmap of switchgear in various voltage levels, which enables customers and industry to reduce carbon footprint and rapidly transition to eco-efficient solutions.

EconiQ TM is Hitachi Energy’s eco-efficient portfolio for sustainability, where products, services and solutions are proven to deliver exceptional environmental performance. Hitachi Energy has placed sustainability at the heart of its Purpose and is advancing a sustainable energy future.

About Hitachi Energy

 

Hitachi Energy is a global technology leader that is advancing a sustainable energy future for all. We serve customers in the utility, industry and infrastructure sectors with innovative solutions and services across the value chain. Together with customers and partners, we pioneer technologies and enable the digital transformation required to accelerate the energy transition towards a carbon-neutral future. We are advancing the world’s energy system to become more sustainable, flexible and secure whilst balancing social, environmental and economic value. Hitachi Energy has a proven track record and unparalleled installed base in more than 140 countries. Headquartered in Switzerland, we employ around 38,000 people in 90 countries and generate business volumes of approximately $10 billion USD.

1 - The RIIO-T2 network price control sets out what the UK gas and electricity transmission network companies are expected to deliver for energy consumers from 2021-2026.

2 - Based on the assumption that a passenger vehicle emits 19 kg CO2 equivalent per 100 km and drives 10,000 km per year.

Contacts

Customer Connect Center

Get to know more