Choose your region and language

Go

Menu

Porto Velho Back-to-back

Customer Story | 2 min read

Stabilizing the grid in northwest Brazil

The Rio Madeira HVDC system is a 6,300 MW ± 600 kV high-voltage direct current transmission system in Brazil built to export electricity from new hydro power plants on the Madeira River in the Amazon Basin to major load centers in southeastern Brazil and a 800 MW back-to-back station located in the northwest.

A consortium consisting of two companies in the Abengoa Group, Inabensa S.A (Spain) and Abengoa Construção Brasil Ltda (Brazil) awarded Hitachi Energy contracts to supply the power equipment for three HVDC stations. The delivery is part of the Brazilian government's Program to Accelerate Development (PAC).

Brazil's power system is about 95 percent hydroelectric. Main load centers are in coastal regions, especially in the southeastern state of São Paulo. 

Hitachi Energy provided two 3,150 MW HVDC converter stations, and an 800-MW HVDC back to back station. 

The 800 MW back-to-back HVDC station transmits power to the surrounding AC network in northwest Brazil. This installation includes capacitor commutated converter (CCC)-type back-to-back converters instead of conventional converters for local electrical loads, providing continuous and even control of voltage and power in the weaker power networks of northwest Brazil.

Main data
Commissioning year: 2013
Configuration: Back-to-back
Power transmitted: 2 x 400 MW
Application: Connecting remote generation
Interconnecting grids