Release of IED Connectivity Package version 3.3.0.0 for Relion® 670 series

Product Release | Västerås, Sweden | 06.07.2019 | 1 min read

The evolution of Relion® 670 series continues with this release.

JULY 3RD, 2019

A new revision of the IED Connectivity Package for the Relion 670 series has been released. The designation of this IED Connectivity Package is 3.3.0.0.

The following feature has been included in the new revision:

Communication security using TLS 1.2
Communication will use TLS version 1.2 for communication security when this Connectivity Package is used together with:

  • PCM600 version 2.9 with Hotfix 20181219 or newer
  • A Relion 670 series version 2.2 (or newer) that is supporting TLS version 1.2

Otherwise, TLS version 1.0 will be used for communications security.

Kind regards,

Krister Hagman, Global Product Manager

All news