Maintenance release of Relion REB500 version 8.2 (8.2.0.5)
Product Release | Västerås, Switzerland | 05.04.2020 | 2 min read
Product Release | Västerås, Switzerland | 05.04.2020 | 2 min read
April 2nd, 2020
The following has been corrected / improved in the new revision:
We recommend users that have experienced issues as described above to update to this release.
Updating to the new firmware does not require any changes in the installed IED Connectivity Packages for REB500. The connectivity packages are available in PCM600 Update Manager.
Order stock as of today will be automatically updated to the new revision. New orders placed on version 8.2 will be delivered with the latest revision 8.2.0.5.
If an earlier version/revision is required, a request shall be made to SA-T sales and an approved deviation shall be in place.
Firmware update of the IED can be performed by the local ABB. If you have any questions related to this maintenance release please contact SA-T Supportline.
Please note that it is very important that you report back to us via SE-mets.submit@abb.com when the update of the concerned IED has been completed. This information is needed to keep our product register updated and to ensure right information to the right local ABB Power Grids units in the future.
Kind regards,
Lars Frisk
Global Lead Product Manager
BL Grid Automation
ABB Power Grids