Choose your region and language

Go

Menu

Furture alternative electricity source:windmill and solar energy-----concept of sustainable resources on a sunny day, Jiangsu,China

Australia’s energy future will be won on grid resilience, not just new megawatts

Blog Post | 05.02.2026 | 6 min read | Bernard Norton

Spend five minutes with any Australian business leader and you’ll hear the same refrain: the energy transition is no longer a question of “if,” it’s a question of “how fast”—and “how reliably.” The country has passed the tipping point. Yet in boardrooms and on building sites, the conversation too often gets stuck on power grid basics such as generation and base load. The real contest over the next few years won’t be won by headlines. It will be won—or lost—on the strength, flexibility and social licence of the grid that ties it all together.

The grid is under stress—and it shows.

Project approvals remain painfully slow, stretching delivery timelines and stranding capital. An ageing transmission backbone built for one-way power flows is being asked to choreograph an increasingly variable mix of solar, wind and storage. That variability, without adequate system strength and inertia, has a destabilizing effect that operators are fighting in real time. The result is a paradox: a nation rich in renewable resources that still faces bottlenecks connecting projects to consumers when and where power is needed most.

Supply chains are the quiet constraint.

Australia is not building its transition in a vacuum; it is competing in a global energy supercycle for the same pool of transformers, high-voltage equipment, power electronics, cables and skilled labour. Lead times have stretched; prices have risen. The antidote is not simply “buy earlier,” but to adopt forward, program of works agreements that bundle demand, give manufacturers clear line of sight, and derisk delivery. This is how we move from transactional procurement to strategic partnership–how we swap uncertainty for throughput.

Households are the ultimate stakeholders.

There is no energy transition without consumer confidence. A cost-of-living crisis has a way of turning abstract system diagrams into very concrete kitchen table anxieties. If the transition is experienced mainly as higher bills or unreliable supply, social licence erodes, and with it the momentum to build what’s needed. The sector must be honest about costs, ruthless about waste, and creative about cushioning impacts—especially for vulnerable customers, but also for communities and landowners. Just as importantly, we need to tell the story of avoided costs: the volatility of imported fuels, the price of climate inaction, and the penalties of deferred maintenance on old assets.

Climate adaptation is no longer a side quest.

Australia’s grid and communities must be prepared for more frequent and severe heatwaves, bushfires, storms and floods. That means building substations and lines to new resilience standards employing digital vegetation management; deploying firesafe right-of-way practices to prevent sparks; and designing redundancy so single point failures don’t cascade. Energy security in a climate stressed world is not just about supply diversity, it’s about infrastructure that can take a punch and keep operating.

Targets are useful; trajectories are decisive.

Reaching 82% renewables by 2030 requires Australia to lock in roughly 5–6 gigawatts of new commitments every year—not in a final hour sprint, but with metronomic regularity. Lumpy, stop start procurement drives up costs and saps capability. A steady cadence, paired with simplified planning and approval processes for projects in the national interest  , lowers risk and invites capital to flow.

Transmission is the multiplier.

We cannot connect what we do not build. Unlocking Renewable Energy Zones, modernising interconnectors and completing priority transmission lines are the highest leverage investments available to policymakers. This is where planning delays bite hardest, and where reform pays the greatest dividend. A faster, more streamlined approvals regime—one that balances environmental stewardship with landholder considerations and national interest—would compress timelines without compromising integrity. When communities see genuine benefits—jobs, community energy, shared infrastructure—they grant the social licence that steel towers alone cannot earn.

The demand side is about to rewire the map.

Electrification of transport, industry and buildings will lift underlying demand even as efficiency improves. On top of that, data centres are emerging as a new class of Australia’s anchor load, with AI and hyper scale data centres increasing energy demand exponentially: power dense, time sensitive and increasingly eager to collocate with clean generation. They can be grid friendly—flexing load, providing demand response, investing in onsite storage—or they can exacerbate congestion and price spikes. Getting the rules right now will determine which path we take.

System strength and inertia need innovation—beyond “more of the same.”

Synchronous condensers have been the default remedy for stabilising weak grids, and they will remain important. But we must move faster toward deploying advanced grid-forming inverters, STATCOMs, and protection schemes leveraging the advances in power electronics and digitalization to protect and manage a more complex energy system of systems. This is not a theoretical exercise; it’s the difference between curtailment and productive output, between “variable equals unstable” and “variable equals manageable.” The technologies exist. What’s required is procurement that rewards performance, not just hardware, and standards that give innovators a clear runway.

What industry and policymakers can do next:

  1. Make grid resilience the North Star.
    Define resilience metrics—restoration time, ride through capability, thermal headroom—and tie funding to meeting them. If every project, from a solar farm to a substation upgrade, has to demonstrate a resilience contribution, we’ll build a system that works on the worst days, not just the best ones.
  2. Institutionalise forward procurement.
    Aggregate demand for critical equipment into multiyear programs with options, not one-off buys. Guarantee volumes where appropriate to pull forward manufacturing capacity and bring down unit costs.
  3. Accelerate planning without eroding trust.
    Set statutory timelines, standardise assessments and create specialist “strike teams” to shepherd complex projects. Pair this with early, authentic community engagement and tangible local benefits. Speed and legitimacy can coexist.
  4. Codify grid forming standards and reward outcomes.
    Update connection and performance standards to reflect an inverter dominant future. Pilot performance based tenders that pay for system strength, inertia and fast frequency response, focusing on technologies that are future fit, flexible and address multiple grid issues in one package.

Australia has all the ingredients to thrive in the new energy economy: worldclass resources, deep pools of capital, sophisticated operators and a public willing to back a credible plan. But success will not come from stacking more megawatts on an old foundation. It will come from a grid that is stronger, smarter and more socially grounded than the one we inherited. The transition’s next phase is not just a race to add capacity; it is a race to add capability. Win that race, and the lights will stay on—affordably, sustainably, and for everyone.

1691640635

Learn more about Hitachi Energy in Australia

Learn more

Bernard Norton
Managing Director, Hitachi Energy Australia

Bernard Norton, Managing Director of Hitachi Energy Australia, leads the company’s growth and industry collaboration to accelerate the nation’s energy transition across key sectors including utilities, mining, renewables, data centres and transport. He champions an inclusive, purpose-driven culture and strong industry partnerships to drive sustainable innovation and impact.