Scegli la tua regione e lingua

Vai

Menu

The opportunity: 

This system is called as MACH. This computerized system is built with the state-of-the-art electronics, microprocessors and digital signal processors, connected by high performance industry standard busses and fiber optic communication links. They operate on very high standard application software developed by Hitachi Energy. As the system is being continuously evolved, the Station Operating and Monitoring System (SOM) is becoming more complex and customized. It requires a great deal of design, testing & verification of HMI, SCADA, Network and Cybersecurity areas.  
  

How you’ll make an impact: 

  • Responsible for detailed project planning, schedule review, budget estimation & review, project scope. 

  • Interfacing with multiple engineering disciplines for technical clarifications, project meetings, internal and customer. 

  • Ensuring the technical scope and inputs are clear to the project team. 

  • Acting as the single point of interface between projects and the Test area, aligning project needs, priorities and follow-ups, inventory management for the test area. 

  • Managing project priorities and resource allocation within the test area, handling Inward and Outward to and from test area. 

  • Knowledge on the quality process connected with the project execution, continuous improvement programs. 

  • Take ownership for the project KPIs such as OTD, COPQ etc, risk and Opportunities meeting, change Management in the projects. 

  • Driving the improvement programs in project and process. 

  • Responsible to ensure compliance with applicable external and internal regulations, procedures, and guidelines. 

  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business. 

Your background: 

  • Bachelor's degree in BE / BTech (EEE). 

  • 4 - 7 years of project management / project lead experience in the industrial control system or SAS. 

  • Control and protection commissioning background.

  • Knowledge in project management concepts. 

  • Experience in Process and ISO audits, quality / L6S / Continuous improvement programs. 

  • Exposure in project planning tools, MS Project. 

  • Proficiency in both spoken & written English language is required. 

Sede Chennai, Tamil Nadu, India
Tipo di lavoro Full time
Esperienza Experienced
Funzione lavorativa Engineering & Science
Contratto Regular
Data di pubblicazione 2026-04-02
Numero di riferimento R0122869

Hitachi Energy

Hitachi Energy è un leader tecnologico globale nell'elettrificazione, che promuove un futuro energetico sostenibile grazie a tecnologie innovative per le reti elettriche, incentrate sul digitale. Oltre tre miliardi di persone dipendono dalle nostre tecnologie per dare energia alla propria vita quotidiana.

Con oltre un secolo di esperienza pionieristica nelle tecnologie mission-critical di alta tensione, trasformatori, automazione ed elettronica di potenza, stiamo affrontando la sfida energetica più urgente del nostro tempo: bilanciare la crescente domanda di elettricità con la decarbonizzazione del sistema energetico.

Con sede in Svizzera e oltre 50.000 persone in 60 paesi, Hitachi Energy genera fatturato per circa 16 miliardi di dollari. Candidati oggi stesso!