Scegli la tua regione e lingua

Vai

Menu

As a System testing engineer, carrying out the configuration of IED’s, development of HMI’s in line with project requirements and testing of Control and relay panels, Substation automation system delivered and actively contribute to the testing team of Grid Automation Systems.

Execute the project IED’s configurations and testing safely following all safety standards of HEIL as well as customer. Report Hazards, Near Misses at work location for records and further improvement.

Carryout the Configurations of IED’s and testing the Control, Protection and SAS panels as per the documented process description and checklists. Continuous interactions with testing Lead and expert help to carry out the testing works effectively.

Report the Configuration and testing project status testing progress & testing plan to testing Lead. Ensure efficient use of the testing assets like Test kits, Tools etc.

Ensures project information of any project is fully taken from testing lead and get all IED’s fully configured and tested in line with customer approved drawings and ready for the project specific testing activities before offering the projects to customer during FAT.

Handing over the marked-up drawings to engineering for preparing the As-build drawing and onward submission to customer to close the project.

Handover the final testing backup CD's, Micro SCADA system backup, IET workplace backup and other backup as per the checklist to lead.

Actively and regularly (Compulsory for every project) provides feedback to Engineering Project Management, manufacturing and quality in way that ensures re-usage of experience.

Follow the key process like Test procedures, Time sheets and STAART Meetings.

Ensure the installed base numerical relays are maintained with minimum revisions by continuously updating the older revisions.

Ensure the usage of the latest tools and latest software versions during  project IED configurations and testing.

Candidates should have strong knowledge of various modulation techniques, SDH/PDH network standards and MPLS-TP networks.

Candidates should be excellent in network designing and troubleshooting.

Should be able to demonstrate customer engagement and solve queries during customer FAT.

Learner who can demonstrate integration of various technologies to deliver turnkey projects.

Should have knowledge of L2 & L3 network devices.

Hands on experience in configuration Linux & Windows based servers for NMS.

Preparing network configuration according to channel plan.

Understanding application or services such as tele protection, tele operation, telephony and data communication.

Continuous learning & acquiring expertise in various protection schemes and Automation system to achieve the higher growth in ‘learning curve’.

Sede Bengaluru, Karnataka, India
Tipo di lavoro Full time
Esperienza Experienced
Funzione lavorativa Engineering & Science
Contratto Regular
Data di pubblicazione 2026-05-13
Numero di riferimento R0126720

Hitachi Energy

Hitachi Energy è un leader tecnologico globale nell'elettrificazione, che promuove un futuro energetico sostenibile grazie a tecnologie innovative per le reti elettriche, incentrate sul digitale. Oltre tre miliardi di persone dipendono dalle nostre tecnologie per dare energia alla propria vita quotidiana.

Con oltre un secolo di esperienza pionieristica nelle tecnologie mission-critical di alta tensione, trasformatori, automazione ed elettronica di potenza, stiamo affrontando la sfida energetica più urgente del nostro tempo: bilanciare la crescente domanda di elettricità con la decarbonizzazione del sistema energetico.

Con sede in Svizzera e oltre 50.000 persone in 60 paesi, Hitachi Energy genera fatturato per circa 16 miliardi di dollari. Candidati oggi stesso!