Scegli la tua regione e lingua

Vai

Menu

The opportunity

Responsible for Configuration of IED’s used in EHV Substations, Development of HMI’s using vendor specific tools and testing of CRP and SAS of EHV substations (above 132kV Voltage level). Ensure that the Substation Automation Projects delivered by HEIL are configured as per the project requirements and tested, put into service on time, meeting highest HEIL quality and OHS standards. Meet or exceed the customer expectations in testing & configuration of IED in line with project requirements.

How you’ll make an impact

  • As a testing and configuration engineer, carrying out the configuration of IED’s, development of HMI’s in line with project requirements and testing of Control and relay panels, Substation automation system delivered and actively contribute in the testing team of Grid Automation Systems.

  • Execute the project IED’s configurations and testing safely following all safety standards of HEIL as well as customer. Reports Hazards, Near Misses at working location back to office for records and further improvement.

  • Ensure that customer relations are managed in an optimal way. Carryout the Configurations of IED’s and testing the Control, Protection and SAS panels as per the documented process description and checklists. Continuous interactions with testing Lead and expert help to carry out the testing works effectively.

  • Report the Configuration and testing project status testing progress & testing plan to testing Lead. Ensure efficient use of the testing assets like Test kits, Tools etc.

  • Ensures project information of any project is fully taken from testing lead  and get all IED’s fully configured and tested in line with customer approved drawings and  ready for the project specific testing activities before offering the projects to customer during FAT.

  • Handing over the marked-up drawings to engineering for preparing the As-build drawing and onward submission to customer to close the project.

  • Handover the final testing backup CD's, Micro SCADA system backup, IET workplace backup and other backup as per the checklist to lead.

  • Actively and regularly (Compulsory for every project) provides feedback to Engineering Project Management, manufacturing and quality in way that ensures re-usage of experience. Follow the key process like  Test procedures ,Time sheets and  STAART Metings.

  • Ensure the installed base numerical relays are maintained with minimum revisions by continuosly updating the older revisions.

  • Ensure the usage of the latest tools and latest software versions during  project IED configurations and testing.

  • Continous learning & acquiring expertise in various protection schemes and Automation system to achieve the higher  growth in  ‘learning curve’.

  • Responsible to ensure compliance with applicable external and internal regulations, procedures, and guidelines.

  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your background

  • Should be a graduate in BE Electrical engineering and should have a minimum of 3 years of experience in testing and commissioning of control and relay panels in projects above 132kV Voltage levels.

  • Should have good knowledge on Power system.

  • Should have hands on experience with 3 Phase injection test kits like Omicron, Doble, Megger, Ponova etc…

  • Should have good knowledge on understanding the schematics of control and relay Panels, primary equipment interlocks.

  • Should be ready for frequent travels all over India and overseas wherever assigned for at least next 5 years.

  • Should have e good knowledge on configuration of HEIL IED’s and competitors IED’s in line with project requirements

  • Should have a minimum of 3 years of experience in commissioning of SAS with IEC61850 standards, IEC101, IEC104, OPC and Modbus protocols.

  • Should have good knowledge on communication protocols listed above.

  • Should have good knowledge on IEC61850 standards, Ethernet, Serial communications.

  • Should have good knowledge on communication protocols such as Modbus, DNP 3.0, IEC 101, IEC 104, OPC,

  • Should have competency on networking, configuration of managed Ethernet switches.

  • Should have hands on experience on Protocol analyzers like IEC browser and network analyzer tools like wire sharks

  • Project drawings & Documents from Test Lead. Project IED configurations plan and testing of panels progress reports on daily basis.

  • Clear with min MOM points during customer FAT. Handing over of project backups once testing is closed.

  • Proficiency in both spoken & written English language is required.

Sede Bengaluru, Karnataka, India
Tipo di lavoro Full time
Modalità di lavoro On-Site
Esperienza Experienced
Funzione lavorativa Engineering & Science
Contratto Regular
Data di pubblicazione 2026-05-23
Numero di riferimento R0131014

Hitachi Energy

Hitachi Energy è leader globale nell’elettrificazione e alimenta l’era dell’elettricità per soddisfare le esigenze energetiche di oggi e dei prossimi 25 anni. Come società del Gruppo Hitachi dedicata al business dell’energia, forniamo tecnologie pionieristiche e mission-critical per alimentare la vita quotidiana di oltre tre miliardi di persone.

Con oltre un secolo di innovazione, stiamo affrontando la sfida energetica più urgente del nostro tempo: guidare l’evoluzione del sistema energetico mondiale per garantire energia abbondante, sicura, accessibile e sostenibile per la generazione di oggi e per quelle che verranno.

Con una base installata senza pari in oltre 140 Paesi, siamo il partner dell’ecosistema di rete nei settori utility, industriale, data center e trasporti. Con sede in Svizzera, impieghiamo oltre 56.000 persone in 60 Paesi e generiamo ricavi per circa 20 miliardi di dollari USA.