Scegli la tua regione e lingua

Vai

Menu

Field Service Engineer - Gas insulated switchgear

Perform Installation & Commissioning site activities for GIS- HV

Services in accordance with the time schedule, quality standards and safety requirements.

Manage On site activities by ensuring availability of material, equipment’s & resources as per the contract specifications.


Main Accountabilities on site:
Installation & Commissioning: Understanding the specification and completing the installation & Commissioning site activities according to the contractual requirement & time schedule.
On Site Service:
Ensure availability of necessary material, equipment & manpower at site by coordinating with the respective stakeholders.
Manage site activities as per the time schedule until completion of the project and inform Field service project Manager or service manager for assistance required for additional resources / material.
The GIS-Supervisor is responsible for the installation work entrusted to him being carried in perfect technical order.
He carries out installation and maintenance work independently.
He instructs, supervises, and controls the installation personnel reporting to him at site.
He is responsible for ensuring compliance with the installation requirements and instructions.
He ensures necessary accident prevention measures are observed; specifically, he abides by the guidelines for work on live system components. He supervises the adherence to the working hours, signs the mom, weekly reports & timesheets and is responsible for forwarding these on.
The GIS Supervisor ensures that the stipulated deadlines are met, i.e., he is responsible for detailed installation planning on-site to enable bottlenecks to be identified in good time, to
formulate proposals for achieving targets and implementing appropriate measures.
Testing: Perform testing for Installed & Commissioned products and provide input to the design team for any modification.
Quality Control: Verifies the application of quality control plan during installation activities
and that the sub contractors are using the safety equipment's as per the requirement.
Documentation: Coordinates with the customer on documentation required and safety coordination.
Information: Inform respective stakeholders on the progress of Installation & Commissioning activities and provide input to the quality team for any non conformance.

Sede Maneja, Gujarat, India
Tipo di lavoro Full time
Modalità di lavoro On-Site
Esperienza Entry Level
Funzione lavorativa Engineering & Science
Contratto Regular
Data di pubblicazione 2026-09-07
Numero di riferimento R0141273

Hitachi Energy

Hitachi Energy è leader globale nell’elettrificazione e alimenta l’era dell’elettricità per soddisfare le esigenze energetiche di oggi e dei prossimi 25 anni. Come società del Gruppo Hitachi dedicata al business dell’energia, forniamo tecnologie pionieristiche e mission-critical per alimentare la vita quotidiana di oltre tre miliardi di persone.

Con oltre un secolo di innovazione, stiamo affrontando la sfida energetica più urgente del nostro tempo: guidare l’evoluzione del sistema energetico mondiale per garantire energia abbondante, sicura, accessibile e sostenibile per la generazione di oggi e per quelle che verranno.

Con una base installata senza pari in oltre 140 Paesi, siamo il partner dell’ecosistema di rete nei settori utility, industriale, data center e trasporti. Con sede in Svizzera, impieghiamo oltre 56.000 persone in 60 Paesi e generiamo ricavi per circa 20 miliardi di dollari USA.