Scegli la tua regione e lingua

Vai

Menu

(empty)

  • Handling of all documents from Internal and External Suppliers. Sending documents for information and approval to both Internal and End Customers.
  • Sort, structure, and put together the Site Documentation, both electronically and in paper form.
  • Delivering Tender Documentation (Bid-submission) to Customer with the inputs from Lead Engineers, Tender Leader, and Dept. Head’s.
  • Profile & upload Drawing files, Manuals, Test Reports, Calculations, etc. required for Bid submission from internal and Suppliers into the Database or common drive, and use various tools like PDL and Binder.
  • Proper follow-up with other departments to submit the documents. Organize the files in a folder structure in the softcopy Binders.
  • Should have experience in contract reading and understand the Customer documentation requirements.
  • Check & upload the Drawing files, Manuals, Test Reports, Calculations, etc. from the Engineers and the sub-suppliers.
  • Upload the documents into the Document Management System (EDMS). Maintain the complete Project Documentation Status.
  • Communicate with the Project Manager and Departments for Clarifications and Suggestions. Proper follow-up with other departments to submit the documents.
  • Distribute the documents to the various departments for review and approval. Send the documents by Transmittal for Customer Review & Approval.
  • Adding the documents to e-Room (web-based database; easy access for members in different locations). Organize the files in a folder structure in the softcopy Binder.
  • Print out the drawings as hard copies and insert them into binders, if needed (This is the installation and Final Plant documentation), and send them to the respective sites.
  • Check & upload the updated drawing files (due to possible changes during on-site installation), and follow all the above steps for new revisions.
  • As-Built documents are printed out as hard copies, inserted into binders, and sent to respective sites (This is the As-Built Documentation). After the Customer Approval, hand over the Project to the After-Sales Department.
  • Responsible for ensuring compliance with applicable external and internal regulations, procedures, and guidelines.
  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Sede Chennai, Tamil Nadu, India
Tipo di lavoro Full time
Modalità di lavoro On-Site
Esperienza Experienced
Funzione lavorativa Project | Program Management
Contratto Regular
Data di pubblicazione 2026-10-06
Numero di riferimento R0138974

Hitachi Energy

Hitachi Energy è leader globale nell’elettrificazione e alimenta l’era dell’elettricità per soddisfare le esigenze energetiche di oggi e dei prossimi 25 anni. Come società del Gruppo Hitachi dedicata al business dell’energia, forniamo tecnologie pionieristiche e mission-critical per alimentare la vita quotidiana di oltre tre miliardi di persone.

Con oltre un secolo di innovazione, stiamo affrontando la sfida energetica più urgente del nostro tempo: guidare l’evoluzione del sistema energetico mondiale per garantire energia abbondante, sicura, accessibile e sostenibile per la generazione di oggi e per quelle che verranno.

Con una base installata senza pari in oltre 140 Paesi, siamo il partner dell’ecosistema di rete nei settori utility, industriale, data center e trasporti. Con sede in Svizzera, impieghiamo oltre 56.000 persone in 60 Paesi e generiamo ricavi per circa 20 miliardi di dollari USA.