Scegli la tua regione e lingua

Vai

Menu

Able to perform the following activities:

  • Review of Tender document, technical specifications and preparation of Design Intent Document
  • Preparation of Protection SLD showing principles, relays and meters
  • Preparation of Functional Design Standards/Descriptions
  • Preparation of Signal list, trip matrix, Logics & Interlocks
  • Review of Vendor drawings and documents (technical vetting of Control & Relay panels, Auxiliary System)
  • Preparation of schematic diagrams for the interface’s equipment in Control & Relay Panel scheme thus providing completeness
  • Preparation of relay ordering information.
  • Preparation of circuit diagrams – New & Existing Set-up (applicable for retrofit projects)
  • Preparation of Cable block diagram
  • Preparation of Cable Schedule & BoQ estimation for ordering
  • Preparation of Wiring/Termination diagrams
  • Preparation of Core sheets
  • Preparation of SCS IO Schedule
  • Panel Engineering Expertise (Layouts, circuit diagram, wiring table, terminal table etc.,) - Preferred
  • Preparation of Voltage drop calculation - Trip & Close coil, LVAC power cable
  • Identification of existing drawings and modifying them using Red and Green markups as per standard requirements
  • Interface knowledge with Primary Equipment, Bay Controller Units /SCADA/RTU/Tele protection are essential
  • Auxiliary Power System design like Low Voltage AC Panel & DC Panel requirements, Aux Tr and Battery & Charger Sizing, ACDC Cable sizing & CB selectivity study.
  • CT / VT Sizing
  • Relay configuration (Preferred)
  • Excellent knowledge in AIS & GIS secondary designs.
  • As Built documentation
  • Co-ordination with other departments like primary, lead engineer, sourcing, C&R factory counterpart & own department control and protection etc. for design progress & completion
  • Vendor Offer Evaluations.  FAT / SAT of primary secondary equipment, system as and when needed.
  • Ensure Ontime delivery of design deliverables & to be vigilant on project schedule impacts.
  • Responsible for obtaining customer approvals for the designs and drawings
  • Technical risk and opportunity assessment and validation
  • Take part in customer meetings / site visits for tender/project clarifications
  • Support and act as interface engineer during erection & commissioning
  • Estimation of engineering effort for each project for costing at tender stage
  • Innovative ideas to reduce Engineering effort
  • Plan, implement, review and continuously improvise quality system
  • Ensure the Safety through design principles which meant for complete project lifecycle.

.

Having an idea about the following activities:

  • Vendor Offer Evaluations.  FAT / SAT of primary secondary equipment, system as and when needed.
  • Ensure Ontime delivery of design deliverables & to be vigilant on project schedule impacts.
  • Technical data sheets verification of equipment’s. Knowledge of equipment, such as circuit breakers, disconnectors, earthing switches, instrument transformers, power transformers, etc
  • Technical risk and opportunity assessment and validation
  • Take part in customer meetings / site visits for tender/project clarifications
  • Support and act as interface engineer during erection & commissioning
  • Estimation of engineering effort for each project for costing at tender stage
  • Innovative ideas to reduce Engineering effort
  • Vendor Offer Evaluations.  FAT / SAT of primary secondary equipment, system as and when needed.
  • Ensure Ontime delivery of design deliverables & to be vigilant on project schedule impacts.
  • Support and act as interface engineer during erection & commissioning
  • Plan, implement, review and continuously improvise quality system & follow OPEX initiatives

Sede Chennai, Tamil Nadu, India
Tipo di lavoro Full time
Modalità di lavoro On-Site
Esperienza Experienced
Funzione lavorativa Engineering & Science
Contratto Regular
Data di pubblicazione 2026-10-06
Numero di riferimento R0139122

Hitachi Energy

Hitachi Energy è leader globale nell’elettrificazione e alimenta l’era dell’elettricità per soddisfare le esigenze energetiche di oggi e dei prossimi 25 anni. Come società del Gruppo Hitachi dedicata al business dell’energia, forniamo tecnologie pionieristiche e mission-critical per alimentare la vita quotidiana di oltre tre miliardi di persone.

Con oltre un secolo di innovazione, stiamo affrontando la sfida energetica più urgente del nostro tempo: guidare l’evoluzione del sistema energetico mondiale per garantire energia abbondante, sicura, accessibile e sostenibile per la generazione di oggi e per quelle che verranno.

Con una base installata senza pari in oltre 140 Paesi, siamo il partner dell’ecosistema di rete nei settori utility, industriale, data center e trasporti. Con sede in Svizzera, impieghiamo oltre 56.000 persone in 60 Paesi e generiamo ricavi per circa 20 miliardi di dollari USA.