Scegli la tua regione e lingua

Vai

Menu

Enabling grid reliability and secure power supply to Ireland and UK

Customer Story | 2 min read

Power transformers are delivering enough energy to power 300,000 homes

Hitachi Energy HVDC Light converter transformers provides the Irish transmission system operator (TSO), EirGrid key equipment to connect the power grids of Ireland and Wales. The East West Interconnector link, connecting to the UK national grid, allows Ireland to access power from right across Europe (via an interconnector from Britain to the continent).

The HVDC Light transformers will increase grid reliability, secure power supply and has the capacity to deliver enough energy to power 300,000 homes. The black start capability makes is possible to quickly restore the power in the event of a blackout.

Hitachi Energy provided seven units of 194 MVA 200 kVDC HVDC Light converter transformers and was responsible for design, manufacturing, testing and installation of the transformers at the converter stations.

The 500-megawatt (MW) transmission connection is the highest capacity link of its kind and establishes an important link between the Irish and U.K. grids, enabling cross-border power flows. The new link also facilitates power trading between the two countries and connects Ireland to the European grid. The link went into operation in 2013.

East West connector
Main data
Customer EirGrid Interconnector Limited
Product HVDC light converter transformers
Application Interconnecting grids
Power rating 194 MVA, 200kV DC, 400kV AC
Location Ireland - U.K
Commissioning 2013
HVDC converter transformers
East West Interconnector